Failed to debug MPC5748G stuck at 98%

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Failed to debug MPC5748G stuck at 98%

1,085件の閲覧回数
naderkhamess
Contributor III

Hello There,

I am working at the moment with Devkit-MPC5748G and was debugging SPI from project from example and made pin connections between DSPI (master) and SPI (slave). And with oscliscope I traced the signals and it was working perfect until I just changed a bit into "0" PushR register to try something. 

Then from this moment I got stuck in debugging and its always says 98%. 

I tried to update the firmware after putting the uC into bootloader mode and copying the "DEBUG-OPENSDA-E200_Pemicro_v110.SDA" file into Bootloader drive. And still I have the same problem. 

I am using S32DS power 2017.R1 and tried to use S32DS power v1.2 and still the same problem. 

I am grateful if someone can help. 

Thanks

4.png

0 件の賞賛
返信
0 返答(返信)