Hi, I have one MPC5748G DevKit Rev D board, but I can't debug it, the IDE report "Device is not detected or may be censored...", can any one help me to solve this problem?
Description:
I tried to debug the MPC5748G DevKit board according to the document "Get Started with the DEVKIT-MPC5748G", I opened the built-in example Hello project from the S32DS IDE, then I tried to debug it, I noticed the LED D53 blinked one time, and then IDE popped up the following dialog:
"Warning: Device is not detected or may be censored. Please enter password in GDB server parameters with debug configurations using the flag -uncensorpassword=n, then restart the debug session."
My board status:
OpenSDA Debug Interface:
S32DS IDE:
and Debug Configurations:
I searched on the NXP Community site and found the following same problems, but they can't solve my problems.
- DEVKIT-MPC5748G Download Error
https://community.nxp.com/t5/NXP-Model-Based-Design-Tools/DEVKIT-MPC5748G-Download-Error/m-p/902870
- Device is not detected or may be censored. DEVKIT-MPC5748G
- uncensorpassword
https://community.nxp.com/t5/S32-Design-Studio/uncensorpassword/m-p/712269
Hello,
I am now confused. So do you see the reset line toggling on Scope after power on reset?
Have a look at following thread on reset escalation recovery with PEMicro:
Best regards,
Peter
no, it can't help me to solve this problem, if the watchdog is not serviced, the board will be reset in a loop, do you have any other suggestion?
Hello,
to exclude reset escalation.
Do you see reset line toggling when measured by scope after power on reset?
There could be active watchdog which is not serviced.
Best regards,
Peter