FEC Ethernet setting RMII mode in MPC5777c

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FEC Ethernet setting RMII mode in MPC5777c

1,511 Views
vignesh_v
Contributor III

I'm trying to transmit packets using MPC5777c the following is the configuration set

My clock XTAL is 25MHZ

per clock  - 100MHZ

void setMacfortheDevice()

{

mac[0] = 0x11;

mac[1] = 0x22;

mac[2] = 0x33;

mac[3] = 0x44;

mac[4] = 0x55;

mac[5] = 0x66;

}

Need to know whether settings are right I'm trying to use mpc5777M ethernet example as ref.

void FEC_Init(void)

{

setMacfortheDevice();

SIU.PCR[99].R = ALTERNATE_2_FUNC|OBE|IBE|SRC|WPE; /* Set to FEC_MDIO */

SIU.PCR[109].R = ALTERNATE_3_FUNC|OBE|WPE; /* Set to FEC_MDC must be strong drive for MDIO & MDC */

SIU.PCR[474].R = PRIMARY_FUNC|OBE|IBE; /* Set to FEC_REF_CLK */

SIU.PCR[252].R = PRIMARY_FUNC|OBE|SRC; /* Set to FEC_TX_EN */

SIU.PCR[248].R = PRIMARY_FUNC|OBE|SRC; /* Set to FEC_TXD[0] */

SIU.PCR[251].R = PRIMARY_FUNC|OBE|SRC; /* Set to FEC_TXD[1] */

SIU.PCR[250].R = PRIMARY_FUNC|IBE|WPE; /* Set to FEC_RXD[0] */

SIU.PCR[253].R = PRIMARY_FUNC|IBE|WPE; /* Set to FEC_RXD[1] */

SIU.PCR[249].R = PRIMARY_FUNC|IBE|WPE; /* Set to FEC_RX_DV */

SIU.FECCR.B.FM = 0; /*Enable RMII Mode*/

FEC.ECR.R = 0x1; // Start reset

while (FEC.ECR.B.RESET) { } ; // Wait for reset to complete

FEC.EIMR.R = 0; // Disable interrupts

FEC.EIR.R = 0xFFFFFFFF; // Clear any interrupts

int i = 0;

for (i = 0; i < 2; i++)

{

// Init tx and rx descriptors

txDesc[i].status = 0x2C00; // Last and transmit CRC

txDesc[i].length = 0;

txDesc[i].bufferPointer = txBuf;

markRxDescEmpty(&rxDesc[i]);

rxDesc[i].bufferPointer = rxBuf[i];

}

// Reset multicast fields

FEC.GAUR.R = 0;

FEC.GALR.R = 0;

FEC.IAUR.R = 0;

FEC.IALR.R = 0;

// Set rx buf size

//FEC.EMRBR.R = sizeof(txBuf);

FEC.EMRBR.R = 1536;

// Set in RMII mode with full frame size 10Mbps

FEC.RCR.R = 0x05EE030C;

// Set RMII speed - operation at 50Mhz /5*2

FEC.MSCR.B.MII_SPEED = 0x5;

// Enable module

FEC.ECR.R = 0x2;

// Enable full duplex

FEC.TCR.R = 0x00000004;

// Enable interrupt

FEC.EIMR.R = 0x02000000;

// Configure a MAC address

FEC.PALR.R = (unsigned long)((mac[0] <<24)|(mac[1] <<16)|(mac[2] <<8)|(mac[3] <<0));

FEC.PAUR.R = (unsigned long)(mac[4] <<24)|(mac[5] <<16); 

// Flag descriptors available to allow reception

FEC.RDAR.R = 0x0100000;

}

Mainly need to know whether my FEC.RCR and MII speed are right?

Thanks & Regards,

Vignesh

Labels (1)
Tags (2)
0 Kudos
8 Replies

1,246 Views
vignesh_v
Contributor III

Hi,

   Ok thanks but I'm unable to view the attachment.

Regards,

Vignesh

0 Kudos

1,246 Views
vignesh_v
Contributor III

Hi Petr,

          I got the attachment . Thanks.

Regs,

Vignesh

0 Kudos

1,246 Views
vignesh_v
Contributor III

Hi,

   The receive Interrupt and transmit interrupt is not hit at any cost also.

Regards,

Vignesh

0 Kudos

1,246 Views
vignesh_v
Contributor III

ok. One more clarification. I have developed based on ref of ethernet demo .. in my target board.

I have configured an interrupt on vector 196 on EIR RXF - for receive interrupt and 195 for TX to indicate tx complete interrupt

. I try to read the status or print the count of tx packets . It either shows large values or zero when I see those in watch buffer kept at a breakpoint. what could be possible cause for the error . IF RCR settings and pin settings are correct is it into some other configuration issue?

I'm using Broard R-Reach cable for transmission where Broadcom chip is used as switch. the link status is established and it shows correct link

but no packets are able to be transmitted which I'm checking basically through wireshark

Regards,

Vignesh

0 Kudos

1,246 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

unfortunately I am not able to help you more. Attached you have one demo example we got from apps team. It was tested on MPC5777C EVB. You can refer to it for the configuration.

Hope it helps.

BR, Petr 

0 Kudos

1,246 Views
vignesh_v
Contributor III

Hi,

SIU.PCR[99].R = ALTERNATE_2_FUNC|OBE|IBE|SRC|WPE; /* Set to FEC_MDIO */

SIU.PCR[109].R = ALTERNATE_3_FUNC|OBE|WPE; /* Set to FEC_MDC must be strong drive for MDIO & MDC */

SIU.PCR[474].R = PRIMARY_FUNC|OBE|IBE; /* Set to FEC_REF_CLK */

SIU.PCR[252].R = PRIMARY_FUNC|OBE|SRC; /* Set to FEC_TX_EN */

SIU.PCR[248].R = PRIMARY_FUNC|OBE|SRC; /* Set to FEC_TXD[0] */

SIU.PCR[251].R = PRIMARY_FUNC|OBE|SRC; /* Set to FEC_TXD[1] */

SIU.PCR[250].R = PRIMARY_FUNC|IBE|WPE; /* Set to FEC_RXD[0] */

SIU.PCR[253].R = PRIMARY_FUNC|IBE|WPE; /* Set to FEC_RXD[1] */

SIU.PCR[249].R = PRIMARY_FUNC|IBE|WPE; /* Set to FEC_RX_DV */

 

SIU.IMUX0.B.MUXSEL6 = 0x01;

SIU.IMUX0.B.MUXSEL5 = 0x01;

SIU.IMUX0.B.MUXSEL4 = 0x01;

SIU.IMUX0.B.MUXSEL3 = 0x01;

SIU.IMUX0.B.MUXSEL2 = 0x01;

SIU.IMUX0.B.MUXSEL1 = 0x01;

SIU.IMUX0.B.MUXSEL0 = 0x01;

SIU.IMUX0.R = SIU.IMUX0.B.MUXSEL6|SIU.IMUX0.B.MUXSEL5|SIU.IMUX0.B.MUXSEL4|SIU.IMUX0.B.MUXSEL3| \

SIU.IMUX0.B.MUXSEL2|SIU.IMUX0.B.MUXSEL1|SIU.IMUX0.B.MUXSEL0;

I tried this for setting up FEC pins is this right . Should there be a high In scope when I probe TX _EN pin.

Can u guide me and correct me if wrong.

Regards,

Vignesh

0 Kudos

1,246 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

there is no need to set IMUX0 for FEC functionality. Rest of setting looks correct, the FEC_REF_CLK is input only.

The TX_EN is driven high when valid nibbles are present on the MII, so during transmission only.

BR, Petr

0 Kudos

1,245 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

FEC.RCR setting looks correct. The MII_SPEED value should be calculated based on FM_PER_CLK.

BR, Petr 

0 Kudos