Ethernet communication example for MPC5744P-257

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Ethernet communication example for MPC5744P-257

727件の閲覧回数
nitinkv
Contributor I

1. Is there a sample code available for MPC5744P Ethernet module with DP83848 PHY for testing on the setup: MPC57XXXMB with MPC5744P-257DS?

2. Could you let me know how to port Ethernet example code available in S32 IDE for other microcontroller like MPC5748G to MPC5744P?

I tried modifying the example code in S32 IDE enet_ping_mpc5748g available in S32 IDE and changed pin muxing and clock configuration to build it for MPC5744P.

When I try to ping to this board with IP 192.168.1.19 from PC with IP 192.168.1.5, I get "Request Timed Out error".

Could you support on how to debug "Request timed out" error?

ラベル(1)
1 返信

494件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hello,

we are dealing with this issue via support case, so I think it is not necessary to use two channels. We will continue in original way and when we resolve the problem, we can post the resolution here.

Regards,

Martin