the function of delay is verified in an application project, and this function is sealed in a library file (xxx.a), when invoke the delay function of the library in another application project, the project process is lost. please see the figure: by the way, invoke other initialization functions in the library, the project is ok, perhaps the interrupts problems of the delay function .
Hi,
how is the delay function implemented? It is possible that in previous project it uses some already configured timer or whatever, but in the new project is not this peripheral initialized or already taken by other functionality.