Erase operation in S32DS tool

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Erase operation in S32DS tool

2,766 Views
TingTing
Contributor II

Hi Developer,

I need your help about S32DS tool.
I want to know how to erase PFlash with S32DS tool? When I try to debug my routine, sometimes the pflash can be erased well, but sometimes not. The error information as followed:
"
Connection from "127.0.0.1" via 127.0.0.1. Connection from port "1914" to 7224
PE-ERROR: Warning. Can't read registers while part is running.
PE-ERROR: Warning. Can't read memory while part is running. @0 (4 bytes)
PE-ERROR: Warning. Can't read memory while part is running. @0 (4 bytes)
PE-ERROR: Warning. Can't read memory while part is running. @0 (4 bytes)
PE-ERROR: Warning. Can't read memory while part is running. @0 (4 bytes)
PE-ERROR: Warning. Can't read memory while part is running. @fbbf20 (4 bytes)
PE-ERROR: Warning. Can't read memory while part is running. @fbc0b0 (4 bytes)
PE-ERROR: Warning. Can't read memory while part is running. @fbc0c0 (4 bytes)
PE-ERROR: Warning. Can't read memory while part is running. @fbbfe8 (4 bytes)
PE-ERROR: Warning. Can't read memory while part is running. @fbc0b0 (4 bytes)
PE-ERROR: Warning. Can't read memory while part is running. @fbc0b0 (4 bytes)
PE-ERROR: Warning. Can't read memory while part is running. @fbc0b0 (4 bytes)
PE-ERROR: Warning. Can't read memory while part is running. @0 (64 bytes)
Interrupt command received. Halting execution.

Device IDCODE is $00000346
Device ID revision is $00000001

Device IDCODE is $00000346
Device ID revision is $00000001

"
It bothered me several days.
Waiting for your help.

PS: My board is MPC5746R.

Many thanks.

BR, Shi Ting Ting

0 Kudos
Reply
3 Replies

2,644 Views
pmrlcbtcphtzjdq
Contributor III

hallo!
I am using a different board but had a similar problem. This entry helped me solve my problems: https://community.nxp.com/t5/S32-Design-Studio/Unable-to-start-debug-session-on-MPC5748G-board-downl...

0 Kudos
Reply

2,761 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

About which tool are you talking? About S32DS debug probe?

If yes, then it does not offer erase possibility. What you have to do is load an empty s-record.

Or buy PEMico or some advance debug tool.

 

best regards,

Peter

0 Kudos
Reply

2,748 Views
TingTing
Contributor II

Hi Petervlna,

My debugger is PEmicro, you can see it in attachment. 

Could you please teach me how to use it to erase flash?

Many thanks!

BR, Shi Ting Ting

0 Kudos
Reply