ESCI not transmitting decimal value 0 in 9 payload frame format

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ESCI not transmitting decimal value 0 in 9 payload frame format

1,222 Views
murugesan_dinak
Contributor II

I'm developing ESCI serial driver for MPC5777c.

This driver is not transmitting decimal value 0 , When it is configured in 9 payload frame format ( 9 character bits and one stop bit).

always setting TN =1, before loading data into the Data register(SDR).

There is no issue if I transmit same character in 8 paylaod format (8 character bit and one stop bit)

Please help me 

2 Replies

1,163 Views
murugesan_dinak
Contributor II

Hi Lukas,

Thanks for your reply.

It is working for me also. The problem is receiver. The receiver which I connected for my testing has some problem receiving this particular character at this mode.

Thanks

Dinakaran 

0 Kudos
Reply

1,163 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Dinakaran,

I can't see problem on my side.

I configured the eSCI in this way:

pastedImage_1.png

And then I simply wrote 0x0 to data register, so payload bits are written as 0 and TN (bit 8) is also 0.

I can measure pulse 0.52ms on oscilloscope. I'm configured baud rate 19200, so 1 start bit + 9 data bits gives:

10*52us = 520us.

Everything is correct from my point of view.

Regards,

Lukas