EEPROM ECC Error injection in MPC5746R

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

EEPROM ECC Error injection in MPC5746R

1,244件の閲覧回数
renjithr
Contributor I

Hi,

I need to test EEPROM for single bit/multi bit error using ECC in MPC5746R. I refereed the following post:

https://community.nxp.com/docs/DOC-332668 

Using this i was able to generate flash fault. Similarly I want to test EEPROM for single bit/multi bit error. 

I tried modifying the address range of flash block to EEPROM block in the above sample code(since it is emulated flash eeprom). But I am not able to inject any fault.So please suggest any methods available.

Thanks,

RR

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 返信

997件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, you may see almost the same thread here:

https://community.nxp.com/thread/458504