Can anyone suggest a descent tool for loading firmware into MPC5748G flash at production time?
Desirable features:
1) Support for downloading and uploading a raw binary file at specified address.
2) Simple user-friendly GUI.
3) Affordable price.
It would also be nice if it would be potent enough to save a device that has entered the dreaded "eternal reset state" that so many threads in this forum is about.
I do not need (or even want) support for debugging.
Best Regards
Ville
Hello,
PLS Development tool is also providing production proved tools for flashing.
FLASH programming with UDE MemTool FLASH programmer
They have different automation capabilities for easy integration into other environments via simple command line tools or script interfaces (e.g. .Net, Phyton, VBA, Perl, ...)
Regards,
Matthias
Hi,
if you are looking for standalone programmer, take a look at:
Next option is:
or
plus
There are also other manufacturers of production flash programmers - I can recall elnec.com, xeltek.com, segger.com...
Regards,
Lukas