Does the SPC5748GGMMJ6  1N81M has CAN FD functionality?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Does the SPC5748GGMMJ6  1N81M has CAN FD functionality?

901 次查看
luissantana
Contributor I


Does the SPC5748GGMMJ6  1N81M has CAN FD functionality?

 

We looked at "Ordering Information" section at the uC DataSheet, but for the "Optional fields", it should have an:

"F" = if CAN FD is available

"S" = HSM (Security Module) Available

 

But our Microcontroller has the letter "G", and we want to make sure that this specific part has CAN FD before ordering the Daughter Board

标签 (1)
标记 (2)
0 项奖励
1 回复

531 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

take a look at:

Is CAN FD available with MPC5748G, now?

Mask set 1N81M is affected by the erratum. The erratum will be fixed on new mask set. I have preliminary information that first samples should be available in late 1H 2016 and qualified mask set should be available in Q4 2016.

Regards,

Lukas

0 项奖励