Does the SPC5748GGMMJ6  1N81M has CAN FD functionality?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does the SPC5748GGMMJ6  1N81M has CAN FD functionality?

903 Views
luissantana
Contributor I


Does the SPC5748GGMMJ6  1N81M has CAN FD functionality?

 

We looked at "Ordering Information" section at the uC DataSheet, but for the "Optional fields", it should have an:

"F" = if CAN FD is available

"S" = HSM (Security Module) Available

 

But our Microcontroller has the letter "G", and we want to make sure that this specific part has CAN FD before ordering the Daughter Board

Labels (1)
Tags (2)
0 Kudos
1 Reply

533 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

take a look at:

Is CAN FD available with MPC5748G, now?

Mask set 1N81M is affected by the erratum. The erratum will be fixed on new mask set. I have preliminary information that first samples should be available in late 1H 2016 and qualified mask set should be available in Q4 2016.

Regards,

Lukas

0 Kudos