Does MPC5777C have a dedicate NVM block that can be accessed without using C55FMC flash controller?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does MPC5777C have a dedicate NVM block that can be accessed without using C55FMC flash controller?

Jump to solution
1,024 Views
ajmerijaimin
Contributor III

I want to set a few "flags or strings" before the reset event and read it back in the next boot up.

We had initially thought of using flash memory that is by using the C55FMC controller. Is there an alternate way for storing smaller data that will retain after reset? because we could not find it in the reference manual.

0 Kudos
Reply
1 Solution
962 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

There's only flash and RAM, I can't see other option.

View solution in original post

3 Replies
993 Views
ajmerijaimin
Contributor III

So we do not have an alternate option other than using SRAM instead of C55FMC?

@lukaszadrapa  can you please confirm?

0 Kudos
Reply
963 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

There's only flash and RAM, I can't see other option.