Does MPC5744 LINFlexd can use the TJA1021 Lin tranceiver?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does MPC5744 LINFlexd can use the TJA1021 Lin tranceiver?

209 Views
ykp3036
Contributor I

Because TJA1021 is the UART to LIN, so can MPC5744 LINFlexd use the TJA1021 Lin tranceiver?Is LINFlexd diffenrent from UART-LIN in physical transmission ?

0 Kudos
1 Reply

190 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

the LINFlexD module offers LIN mode, supports LIN protocol version 1.3, 2.0, and 2.1 and the TJA1021 is LIN transceiver, connection is normally possible using TXD and RXD pins. 

PetrS_0-1677487586450.png

The transmit data stream of the protocol controller at the transmit data input (TXD) is converted by the TJA1021 into a bus signal. The receiver detects the data stream at the LIN bus input pin and transfers it via pin RXD to the microcontroller.

BR, Petr

0 Kudos