Does DEVKIT MCP5748G feature HSM?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does DEVKIT MCP5748G feature HSM?

2,088 Views
fab_
Contributor II

Hi,

I'm wondering if the DEVKIT-MCP5748G is featured with HSM. If I'm correct, the datasheet says only MCP5748GS is equiped with a HSM.

In case it isn't equiped with HSM, is there an alternative module or feature for data encryption on the MCU?

Thanks for your help.

Cheers, Fab_

Labels (1)
Tags (1)
0 Kudos
Reply
3 Replies

1,929 Views
ankur_kala
NXP Employee
NXP Employee

No Devkit is HSM enabled. In case you want to work with HSM enabled parts, you need to get in touch with your local sales representative. HSM enabled parts come with security firmware programmed.

Regards,

Ankur

1,928 Views
fab_
Contributor II

Hi Ankur, thanks for the quick response. Too bad the DEVKIT doesn't have the feature.

Also, thanks to petervlna‌ for you effort.

Kind regards,

Fabian

0 Kudos
Reply

1,929 Views
petervlna
NXP TechSupport
NXP TechSupport

Hi,

Not only S version has HSM. Also T and H versions:

pastedImage_1.png

I have check the DEVKIT here in lab and it is equiped with S version. So there is HSM available on DEVKIT.

However I cannot see any additional information about HSM availability on our web page.

regards,

Peter

0 Kudos
Reply