Documentation for the Cross Triggering Unit in MPC5675K

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Documentation for the Cross Triggering Unit in MPC5675K

1,311件の閲覧回数
JChMathae
Contributor II

Hello,

 

 

Is there a more complete documentation for the Cross Triggering Unit than the short one provided in the MPC5675K User Manual?

 

We are trying to configure it for ADC use, and a comprhensive description of its modes would be welcomed.

 

Thank you.

 

Best regards.

 

 

Jean-Christophe MATHAE

CIRTEM
http://www.cirtem.com

bâtiment Pointe Bleue
1389 L'Occitane

  31670 LABEGE

  France

ラベル(1)
0 件の賞賛
2 返答(返信)

673件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

I am not aware anything more is available except of Modules description given in the RM.

I can give you basic example which shows synchronization between FlexPWM, CTU and ADC modules.

The FlexPWM Submodule 0 is initialized to generate PWM signal, and rising edge of PWM B0 signal is used to generate trigger signal for CTU module. The CTU module sends one command to ADC. Single conversion mode is used, and ADC0 ch0 is sampled. The conversion result is used to modify PWM B0 rising egde position within the ADC EOC interrupt.

Hope it helps.

Regards,

Petr

0 件の賞賛

673件の閲覧回数
JChMathae
Contributor II

Thank you very much Petr.

(Excuse me for being so late)

Best Regards.

Jean-Christophe MATHAE

0 件の賞賛