Do you have a certificate of conformance to test plan ISO 16845 for the MPC5668G CAN?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Do you have a certificate of conformance to test plan ISO 16845 for the MPC5668G CAN?

536 Views
raphaelvanstrae
Contributor I

My customer asks a certificate that shows that the CAN control unit of the microcontroller MPC5668G

complies with the test plan of ISO 16845.

0 Kudos
1 Reply

432 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

attached. Notice that CAN conformance test was done only on MPC5604B derivative because the same module is used on more devices. The CAN conformance test is done only for module, not for all derivatives.

Regards,
Lukas

0 Kudos