Hello
I'm trying to disable the JTAG on MPC5567.
I've tried to erase the shadow flash : The MCU no longer boot from internal flash ( Bootcfg = 0 0 )
Changing the shadow flash y JTAG doesn't work well ( get several part bricked trying to change the shadow flash with a Cyclone tool)
Question :
1) Reading the 55667RM doesn't explain why MCU doesn't start when the shadow flash has been erased ( it does on 5644A)
2) What shall really be changed to secure the MCU ? ( block the JTAG to avoid a reading of the internal flash)
Regards
Tnkas
If MCU is censored, it behaves according following table:
SIU_RSR(BOOTCFG[0:1]) , boot mode, internal flash state, nexus state
00, internal boot, enabled, disabled
01, serial boot, disabled, enabled
10, external boot, disabled, enabled
11, external boot, disabled, enabled
I don’t see any reason why fully erased shadow flash should block booting from internal flash, I would rather guess you have changed something else. I would recommend to only modify serial passcode and control word with private password in order not to permanently lock the device.
Pay attention to following appnote: