Disable a CACHE at BOOT on MPC55XX for a specific EBI ADDRESS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Disable a CACHE at BOOT on MPC55XX for a specific EBI ADDRESS

3,249 Views
abelussi
Contributor III

The goal is to update the software program into the flash of MPC5554 if requested by operator before launch the program alreay installed at address 0x20000 of internal flash.

At the start-up into my main() procedure (0x0000 of internal flash) I have to acces to as specific size of memory space ,connected to FPGA by EBI bus, by the following routine:

#define REG_READ16(addr)        (*(volatile uint16_t*)(addr))

The problem is that when I try to access at this specific address the cache added also next 8 address data request

I disable the cache completely by the following instruction (disable all cache)

                asm("mfspr r3, l1csr0");

                asm("clrrwi r3, r3, 1");

                asm("msync ");

                asm("isync ");

                asm("mtspr l1csr0, r3");

                asm("isync ");

the read access is OK ........  but I have problem with procedure that init internal flash device:

returnCode = pFlashInit( &ssdConfig );

not works

 

In the main application (that use Integrity) by BSP I set this size of memory as:

#define FPGA_REG_BEGIN 0x3FD00000

#define FPGA_REG_END     0x3FD3FFFF

 

PhysicalRange BSP_PhysicalMemoryRanges[] = {

/* Attributes, PhysicalSpcaeNumber, First, Last, Type, name */

/* Same as "Basic memory regions" in ppc5554.h */

{ MEMORY_RWE | MEMORY_VOLATILE | MEMORY_IOCOHERENT, 0, FPGA_REG_BEGIN, FPGA_REG_END,  };

 

My question: Is possibile to disable not all cache but only a for a specific address also into my main procedure ?

 

Could you suggest me an idea ?

Thanks in advanced

 

 

 

0 Kudos
Reply
10 Replies

3,243 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, you may configure multiple address ranges by MMU TLB entries and use cache-inhibited attribute for areas where access in not supposed to be cached.

Following tool could be useful:

https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/MMU-Assist-Register-CONFIGURATOR/ta-p/1110436

0 Kudos
Reply

3,238 Views
abelussi
Contributor III

Thanks David

I set the TLB as below , but I see that the cache is not disable yet.

 

; Modify Entry 6 to specify 0x3fd00000-0x3fd3ffff for FPGA registers

lis r12, %hi(0x10060000) ; 
mtspr mas0, r12 ; 

lis r12, %hiadj(0xc0000400) ; 
addi r12,r12,%lo(0xc0000400) ; 
mtspr mas1, r12 ; 

lis r12, %hiadj(0x3fd0001e) ; 
addi r12,r12,%lo(0x3fd0001e) ; 
mtspr mas2, r12 ; 

lis r12, %hiadj(0x3fd00005) ; 
addi r12,r12,%lo(0x3fd00005) ; 
mtspr mas3, r12 ; 

tlbwe ; Set TLB entry

tlbsync

 

Do you have any other suggestion ?

Thanks in advanced

0 Kudos
Reply

3,235 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Are you using write-through or copy-back mode?

0 Kudos
Reply

3,225 Views
abelussi
Contributor III

write-through

0 Kudos
Reply

3,214 Views
abelussi
Contributor III

How can set the VOLATILE mode ?

 

Thanks

0 Kudos
Reply

3,199 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

i am sorry, I don't understand context.

0 Kudos
Reply

3,194 Views
abelussi
Contributor III

Sorry for mistake...

As explained before I try to read by the simple instruction (see below) the data into the FPGA by EBI bus.

#define REG_READ32(addr) (*((volatile uint32_t*)(addr)))

#define FPGA_RAM_TEST_REG  0x3fd23fe0

int main(int argc, char *argv[])
{
uint16_t value = 0;
value = REG_READ32(FPGA_RAM_TEST_REG);

}

 

I initialize the EBI bus as below, but when I try to read a data at the address (0x3FD23FE0),  I can't see the chip select CSO in the oscilloscope. CSO not move. In the post before I talk about the cache (disable/enable), but I'm wrong because the access to memory it's coming from the emulator memory window left open for mistake.

Could you check if are there some error in the setting ?

Thanks in advanced

 

Setting-1:

; Modify Entry 6 to specify 0x3fd00000-0x3fd3ffff for FPGA registers

lis r12, %hi(0x10060000) 
mtspr mas0, r12 

lis r12, %hiadj(0xc0000400)
addi r12,r12,%lo(0xc0000400)
mtspr mas1, r12 

lis r12, %hiadj(0x3fd0001e) 
addi r12,r12,%lo(0x3fd0001e) 
mtspr mas2, r12

lis r12, %hiadj(0x3fd00005) ; Start of FPGA, physical address
addi r12,r12,%lo(0x3fd00005) ; and permission bits SW, SR
mtspr mas3, r12 ; Set MMU Assist Register 3

tlbwe


; Invalidate TLB entries 7..31
li r12, 0x00000000 ; Set to zero
mtspr mas1, r12
mtspr mas2, r12 
mtspr mas3, r12 

li r11, 7
lis r12, %hi(0x01070000) ; Entry Select (ESEL) = 7, TLB Select (TLBSEL) = 1
settlb: mtspr mas0, r1
tlbwe 

addis r12,r12,%hi(0x00010000) 
addi r11,r11,1
cmplwi r11, 32 
blt settlb ;

tlbsync

 

Setting-2:

;Configure I/O pins for external address bus 

li r12, 0x0440
lis r11, %hi(0xc3f90000)
; Set Pad Configuration Registers 4..27 as ADDR[8..31]
; Set PA = 1 (primary function)
; Set DSC = 0b01 = 20pF drive strength
sth r12, 0x48(r11) ; 0xc3f90048 = 0x0440
sth r12, 0x4a(r11) ; 0xc3f9004a = 0x0440
sth r12, 0x4c(r11) ; 0xc3f9004c = 0x0440
sth r12, 0x4e(r11) ; 0xc3f9004e = 0x0440
sth r12, 0x50(r11) ; 0xc3f90050 = 0x0440
sth r12, 0x52(r11) ; 0xc3f90052 = 0x0440
sth r12, 0x54(r11) ; 0xc3f90054 = 0x0440
sth r12, 0x56(r11) ; 0xc3f90056 = 0x0440
sth r12, 0x58(r11) ; 0xc3f90058 = 0x0440
sth r12, 0x5a(r11) ; 0xc3f9005a = 0x0440
sth r12, 0x5c(r11) ; 0xc3f9005c = 0x0440
sth r12, 0x5e(r11) ; 0xc3f9005e = 0x0440
sth r12, 0x60(r11) ; 0xc3f90060 = 0x0440
sth r12, 0x62(r11) ; 0xc3f90062 = 0x0440
sth r12, 0x64(r11) ; 0xc3f90064 = 0x0440
sth r12, 0x66(r11) ; 0xc3f90066 = 0x0440
sth r12, 0x68(r11) ; 0xc3f90068 = 0x0440
sth r12, 0x6a(r11) ; 0xc3f9006a = 0x0440
sth r12, 0x6c(r11) ; 0xc3f9006c = 0x0440
sth r12, 0x6e(r11) ; 0xc3f9006e = 0x0440
sth r12, 0x70(r11) ; 0xc3f90070 = 0x0440
sth r12, 0x72(r11) ; 0xc3f90072 = 0x0440
sth r12, 0x74(r11) ; 0xc3f90074 = 0x0440
sth r12, 0x76(r11) ; 0xc3f90076 = 0x0440

; Set Pad Configuration Registers 28..43 as Data[0..15]
sth r12, 0x78(r11) ; 0xc3f90078 = 0x0440
sth r12, 0x7a(r11) ; 0xc3f9007a = 0x0440
sth r12, 0x7c(r11) ; 0xc3f9007c = 0x0440
sth r12, 0x7e(r11) ; 0xc3f9007e = 0x0440
sth r12, 0x80(r11) ; 0xc3f90080 = 0x0440
sth r12, 0x82(r11) ; 0xc3f90082 = 0x0440
sth r12, 0x84(r11) ; 0xc3f90084 = 0x0440
sth r12, 0x86(r11) ; 0xc3f90086 = 0x0440
sth r12, 0x88(r11) ; 0xc3f90088 = 0x0440
sth r12, 0x8a(r11) ; 0xc3f9008a = 0x0440
sth r12, 0x8c(r11) ; 0xc3f9008c = 0x0440
sth r12, 0x8e(r11) ; 0xc3f9008e = 0x0440
sth r12, 0x90(r11) ; 0xc3f90090 = 0x0440
sth r12, 0x92(r11) ; 0xc3f90092 = 0x0440
sth r12, 0x94(r11) ; 0xc3f90094 = 0x0440
sth r12, 0x96(r11) ; 0xc3f90096 = 0x0440

; Set Pad Configuration Registers 44..59 as Data[16..31]
sth r12, 0x98(r11) ; 0xc3f90098 = 0x0440
sth r12, 0x9a(r11) ; 0xc3f9009a = 0x0440
sth r12, 0x9c(r11) ; 0xc3f9009c = 0x0440
sth r12, 0x9e(r11) ; 0xc3f9009e = 0x0440
sth r12, 0xa0(r11) ; 0xc3f900a0 = 0x0440
sth r12, 0xa2(r11) ; 0xc3f900a2 = 0x0440
sth r12, 0xa4(r11) ; 0xc3f900a4 = 0x0440
sth r12, 0xa6(r11) ; 0xc3f900a6 = 0x0440
sth r12, 0xa8(r11) ; 0xc3f900a8 = 0x0440
sth r12, 0xaa(r11) ; 0xc3f900aa = 0x0440
sth r12, 0xac(r11) ; 0xc3f900ac = 0x0440
sth r12, 0xae(r11) ; 0xc3f900ae = 0x0440
sth r12, 0xb0(r11) ; 0xc3f900b0 = 0x0440
sth r12, 0xb2(r11) ; 0xc3f900b2 = 0x0440
sth r12, 0xb4(r11) ; 0xc3f900b4 = 0x0440
sth r12, 0xb6(r11) ; 0xc3f900b6 = 0x0440

; Set Pad Configuration Register 62 as RD/WR
sth r12, 0xbc(r11) ; 0xc3f900bc = 0x0440
; Set Pad Configuration Register 63 as /BDIP
sth r12, 0xbe(r11) ; 0xc3f900be = 0x0440

; Set PA = 1 (primary function)
; Set DSC = 0b01 = 20pF drive strength
; Set WPE and WPS
li r12, 0x0443

; Set Pad Configuration Registers64..67 as WE[0..3]
sth r12, 0xc0(r11) ; 0xc3f900c0 = 0x0443
sth r12, 0xc2(r11) ; 0xc3f900c2 = 0x0443
sth r12, 0xc4(r11) ; 0xc3f900c4 = 0x0443
sth r12, 0xc6(r11) ; 0xc3f900c6 = 0x0443
; Set Pad Configuration Register 68 as OE
sth r12, 0xc8(r11) ; 0xc3f900c8 = 0x0443
; Set Pad Configuration Register 69 as TS
sth r12, 0xca(r11) ; 0xc3f900ca = 0x0443
; Set Pad Configuration Registers 0..3 as /CS[0..3]
sth r12, 0x40(r11) ; 0xc3f90040 = 0x0443
sth r12, 0x42(r11) ; 0xc3f90042 = 0x0443
sth r12, 0x44(r11) ; 0xc3f90044 = 0x0443
sth r12, 0x46(r11) ; 0xc3f90046 = 0x0443

 

Setting-3:


; Set External Bus Interface (EBI)
; CS0 selects FPGA registers at 0x3fd00000, size 0x40000

lis r12, %hiadj(0x3fd00043) ;
addi r12,r12,%lo(0x3fd00043) ;

stw r12, 0x4010(r11) ;0xc3f84010 = (0xc3f80000+(0x43 or 0x843))

; Write EBI Option Register Bank 0 (EBI_OR0)
; 0xfffc0000 = Address Mask (AM)
; 0xf0 = Cycle Length (SCY) = 0xf
lis r12, %hiadj(0xfffc00f0) 
addi r12,r12,%lo(0xfffc00f0) 
stw r12, 0x4014(r11) 

0 Kudos
Reply

3,160 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

A principle could be correct (if i understand what you actually want to achieve). I haven't checked values.

Note to tlbwe instruction - in this sequence isync is required after and msync before

0 Kudos
Reply

3,133 Views
abelussi
Contributor III

I solve by set the "VALID" bit of mas1 register as "This TLB entry is invalid"

instead of "This TLB entry is invalid"

 

Could you give me an explanation ?  .......... to understand my error

Thanks

0 Kudos
Reply

3,107 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

I haven't understand your description as it does not make sense.

VALID bit needs to be set to make the entry valid (i.e. active), otherwise it is invalid (inactive).

0 Kudos
Reply