Differences between SPC5748GHK0AMMJ6 and SPC5748CBK0AMMJ6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Differences between SPC5748GHK0AMMJ6 and SPC5748CBK0AMMJ6

Jump to solution
486 Views
ZhaozhangChen
Contributor I

Hi

      Can you tell me that there are other differences between SPC5748GHK0AMMJ6 and SPC5748CBK0AMMJ6 apart from the number of cores and USB, do they need to be compatible with hardware design? Are they PintoPin?

0 Kudos
Reply
1 Solution
462 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

This information is in datasheet:

petervlna_0-1665995393288.png

And yes, they are pin to pin compatible.

Best regards,

Peter

 

View solution in original post

0 Kudos
Reply
2 Replies
463 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

This information is in datasheet:

petervlna_0-1665995393288.png

And yes, they are pin to pin compatible.

Best regards,

Peter

 

0 Kudos
Reply
477 Views
ZhaozhangChen
Contributor I

Is the IO signal Excel in the attachment of SPC5748G RM shared with SPC5748C?

0 Kudos
Reply