DSPI of MPC5746R

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DSPI of MPC5746R

617 Views
qm1013
Contributor III

hello, do you have the demo software which configured the DSPI in  simplified SPI mode without TXFIFO and RXFIFO ?

I have some problems about the configuration of DSPI in simplified SPI mode .

Below is the MPC5744P SPI Demo:

SPI_2.PUSHR.PUSHR.R = 0x00001234; /* Initialize slave DSPI_2's response to master */
SPI_1.PUSHR.PUSHR.R = 0x08015678; /* Transmit data from master to slave SPI with EOQ */
read_data_DSPI_2(); /* Read data on slave DSPI */
read_data_DSPI_1(); /* Read data on master DSPI */

I not sure that if the transmit commands need to write to PUSHR register? And about 0x5678, is the 0x78 transmit first or the 0x56 transmit first?

Tags (2)
0 Kudos
Reply
1 Reply

503 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

take a look at https://community.nxp.com/docs/DOC-343219 

Regards,

Lukas

0 Kudos
Reply