DMA scatter and gather

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DMA scatter and gather

787 Views
ceciliac
Contributor III

Hi,

What is the difference between using DMA scatter and gather and channel linking?

Does scatter and gather require an additional DMA service request to continue with the second TCD?

I am doing some tests on MPC5746R (triggering DMA transfers from eTPU) and as far as I understand with channel linking I can perform e g two transfers (two eTPU variables) on one service request whereas  with scatter and gather only one transfer is performed per DMA service request, is this correct?

Thanks,

Cecilia

1 Reply

626 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi,  
Channel linking means that after end of major loop of certain channel, another channel is triggered.


Scatter-gather is more universal feature but brings additional transfer on internal bus (it is needed to load new descriptor). On the other hand will occupy only one channel, because new TCD replaces original one. This way you can chain any amount of TCDs. Regarding DMA service request - if can be configures both way acording to START bit of newly loaded TCD, thus it can be immediately triggered (START = 1) or it'll be triggered by another DMA request (START = 0).