Core Voltage (LVD & HVD) monitoring(MPC5746) using MCAL(AUTOSAR)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Core Voltage (LVD & HVD) monitoring(MPC5746) using MCAL(AUTOSAR)

681 Views
kasham_babu
Contributor I

Hello,

I need some information about handling of  1.2V core voltage LVD/HVD operations (MPC5746C) using MCAL (AUTOSAR).if we can't handle using MCAL configurations, Please provide some information about how to monitoring the Core voltages and logging DTCs.  

Any additional information on this topic is useful.

 

Thanks in Advance.

0 Kudos
1 Reply

570 Views
frantisekdobes
NXP Employee
NXP Employee

Hello,

MCAL supports configuration of  PMCDIG_MCR register in McuPmcMisc_Config configuration container:

 pastedImage_1.png

There is also supported configuration of HVD/LVD resets in McuResetConfig configuration container:

pastedImage_2.png

 

For status there can be read directly the Supply Gauge Status Register (PMCDIG_SGSR) which provides information about LVD/HVD (there is no API in MCAL).

Best Regards,

Frantisek