Can be used as external interrupt port D of MPC5604P?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can be used as external interrupt port D of MPC5604P?

423件の閲覧回数
taokang
Contributor III

Dear NXP engineer:

    I want to use  the portD as a external interrupt,as you know,The SIUL only supports 32 external interrupts,As shown in the figure below

UC截图20170402170549.png

So,I have two question:

1.Can be used as external interrupt port D?

2.If it can’t,Want to use the port D as an external interrupt source is there any way can replace?

Please give me your valuable answer!

Thanks!

0 件の賞賛
1 返信

313件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, only those pins having EIRQ functionality can be used. Port D does not have such one.

pastedImage_2.png

0 件の賞賛