Can be used as external interrupt port D of MPC5604P?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can be used as external interrupt port D of MPC5604P?

485 Views
taokang
Contributor III

Dear NXP engineer:

    I want to use  the portD as a external interrupt,as you know,The SIUL only supports 32 external interrupts,As shown in the figure below

UC截图20170402170549.png

So,I have two question:

1.Can be used as external interrupt port D?

2.If it can’t,Want to use the port D as an external interrupt source is there any way can replace?

Please give me your valuable answer!

Thanks!

0 Kudos
Reply
1 Reply

375 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, only those pins having EIRQ functionality can be used. Port D does not have such one.

pastedImage_2.png

0 Kudos
Reply