Can SPC5746CBK1AMKU6 replace SPC5744BFK1ACKU2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can SPC5746CBK1AMKU6 replace SPC5744BFK1ACKU2

419 Views
3150100789
Contributor I

Recently I am working on a project, I have designed the hardware circuit diagram and the underlying driver, and now I find that the original main control chip SPC5744BFK1ACKU2 is out of stock, can it be replaced by other chips, such as SPC5746CBK1AMKU6, they have the same number of pins.

最近我在学校里研究课题设计整车控制器,里面用到了芯片SPC5744BFK1ACKU2,已经完成了硬件电路设计和底层软件的搭建,现在发现芯片已经没有库存,市面上买不到,我想问下能用同系列的SPC5746CBK1AMKU6代替吗,两者都是176pin的,就是一些参数不同。

0 Kudos
2 Replies

411 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Yes, I see no issue in replacement. It will fit with no issues.

Only difference is in flash size.

Best regards,
Peter

0 Kudos

407 Views
3150100789
Contributor I

thank you!

0 Kudos