Can FEC memory be used as general-purpose RAM?

取消
显示结果 
搜索替代 
您的意思是: 
已解决

Can FEC memory be used as general-purpose RAM?

跳至解决方案
564 次查看
EAlepins
Contributor V

In the MPC5777C, I will not be using the FEC Ethernet controller. However, it would be nice if I could increase the total internal RAM such that the cores/applications could put variables in the FEC internal RAMs. Is that possible?

Also, what is the size and number of RAMs embedded in the FEC?

Thanks.

标签 (1)
标记 (4)
0 项奖励
1 解答
443 次查看
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi,

I have tried it and it seems FEC MIB RAM can be used as "normal" RAM when FEC is disabled. Is is small area 0xFFF4_C200h–0xFFF4_C3FFh and it can only be accessed by 32-bit. Also access time is expected to be slower (access over PBRIDGE).

FEC FIFO RAM does not seems to be possible to access directly.

在原帖中查看解决方案

0 项奖励
1 回复
444 次查看
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi,

I have tried it and it seems FEC MIB RAM can be used as "normal" RAM when FEC is disabled. Is is small area 0xFFF4_C200h–0xFFF4_C3FFh and it can only be accessed by 32-bit. Also access time is expected to be slower (access over PBRIDGE).

FEC FIFO RAM does not seems to be possible to access directly.

0 项奖励