CW2.10,SPC5605b auto connect problem?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CW2.10,SPC5605b auto connect problem?

908 Views
wuxuliang
Contributor II

   CW2.10,My design use SPC5605bmll6,When debuging,if CPU setting is autodetect,in high level load dialog, Program binary image into Flash using default Algorithm for Selected Device is MPC5606BK(Autodetect).

    If CPU setting is MPC5605B,in high level load dialog, Program binary image into Flash using default Algorithm for Selected Device is MPC5606B.While I Add Register in Variables window,it is all MPC5607B register.

  1.  I what to know that is OK or not.

  2.At the same time,In project I cannot change all PCR.R.but In memory window,I can write data in sram(0x40000000).and ex-clock is OK.

need help

THANKS 

Tags (1)
0 Kudos
1 Reply

517 Views
martin_kovar
NXP Employee
NXP Employee

Hello,

what do you mean by:

Program binary image into Flash using default Algorithm for Selected Device is MPC5606BK(Autodetect).

    If CPU setting is MPC5605B,in high level load dialog, Program binary image into Flash using default Algorithm for Selected Device is MPC5606B

Where did you check that this algorithm was used?

About your second question, please read my answer in your second thread:

https://community.nxp.com/thread/445957 

Regards,

Martin

0 Kudos