CW11.1 for MPC56X Problem1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CW11.1 for MPC56X Problem1

2,268 Views
NXP_Hongyu
Contributor I

Capture.PNGwhen i installed the CW11.1, i can't create a new project for MPC56X, because i can't find relevant device

 

0 Kudos
Reply
11 Replies

2,262 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

it was necessary to select "Qorivva" (this was a nickname for MPC5xxx devices in the past) during the  installation:

lukaszadrapa_0-1632307753339.png

To add support to existing installation, open Help -> Install New Software

and select:

lukaszadrapa_1-1632307858493.png

Regards,

Lukas

1,964 Views
JOE_1209
Contributor III

Hi Lukas,

I am also using the chip MPC5602P and I have followed the instruction to update the Qorivva Support & MCU v11.1 Update for Qorivva. However, when I created a new project for MPC5602P,  the component inspector is blank. I assume there is no SDK S32PA support for MPC5602P? I also tried S32 design studio power architecture, the component inspector is blank as well

S32 Design Studio問題.PNG

Regards,

Joe

0 Kudos
Reply

1,949 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

yes, that's correct. There's no SDK for MPC56xx family of devices. We provided Autosar MCAL only:

https://www.nxp.com/design/automotive-software-and-tools/autosar:AUTOSAR-HOME

Regards,

Lukas

 

0 Kudos
Reply

1,935 Views
JOE_1209
Contributor III

Hi Lukas,

 

Thank you for the reply. I installed the files

1. STUDIO_14.0.0_2013-02-26

2. MPC560XP_MCAL4.0_RTM_1.0.0_signed

3. MPC560XP_MCAL4.0_RTM_HF1_1.0.0_signed

For the MCAL4.0 RTM, I installed them under the path of "C:\EB\tresos\plugins"

file directory.PNG

When I clicked file -> import -> Existing Project into Workspace on Tresos studio, I selected "MPC560XP_MCAL4.0_RTM_1.0.0_Integration_Application" as root directory. (which then be copied into workspace). Then I clicked SampleApplication (PA, XPC560XP), it prompted a warning showing T2D11M10I0R0 is not installed. Where should I move all the files with T2D11M10I0R0 ending? So the Tresos Studio can load the configuration.

EBtresos.PNG

My intent here is to only configure the low level driver and pin configuration. no need for OS.

 

Best Regards,

Joe 

0 Kudos
Reply

1,831 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Joe,

I'm sorry for delayed response caused by Christmas holidays. This is for another team, so if it is still not resolved, please create new ticket here and it will be assigned to them:

https://support.nxp.com/

Thanks,

Lukas

0 Kudos
Reply

1,827 Views
JOE_1209
Contributor III

Hi Lukas,

Happy 2022, I created a new post and Nam is helping me with the issue

Thanks,

Joe

0 Kudos
Reply

2,248 Views
NXP_Leo
Contributor II

Hi 

I operate according to your instructions, i meet a new issue below:

Capture.PNG

I disable the 1.0.3 version of buildtools, then it can continue again, but i don't know whether this will influence my developpment.

0 Kudos
Reply

2,246 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

That should be ok, it's just older version which is not needed.

Regards,

Lukas

0 Kudos
Reply

2,230 Views
NXP_Leo
Contributor II

Capture.PNG

MCU above is what i use, but i don't know which family i should select from item below:

Capture1.PNG

0 Kudos
Reply

2,225 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

if you really have SPC5604P34/SPC560P40, you are talking to wrong company. These are parts from ST. Please contact www.st.com

Regards,

Lukas

0 Kudos
Reply

2,241 Views
NXP_Leo
Contributor II

Thanks for your support!

0 Kudos
Reply