CAN length problem MPC5604

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CAN length problem MPC5604

Jump to solution
1,504 Views
xuuurraa
Contributor II

Hi, my name is Xavier. 

I have a problem with CAN interruption with MPC5604.

In the first message, i have the interruption, then I read the length of the message , but when i recieve the next message the interruption don´t occur again, only occur when change to another buffer or without reading the length of the message.

I read it with this command:

dummy = CAN_0.BUF[buffer_lectura].CS.B.LENGTH;

This is my code:

#include "MPC5604P.h"
#include "IntcInterrupts.h"
#include "INIT.h"
#include "Definicions.h"
#include "Variables_globals.h"
#define LLIBRERIA


//++++++++++++++++++++++++++++INTERRUPCIONS++++++++++++++++++++++++++++++++++++++++++++++++++
/*----------------- Rutina de servei a la interrupcio del CAN0 BUFFER 8-11 ------------------
/* Interrupcio del PC per a carregar totes les taules en memoria
-------------------------------------------------------------------------------------------*/
static void CAN0_ISR_TAULES (void) {

if (nova_taula == 0) {
nova_taula = 1;
if (CAN_0.IFRL.B.BUF08I == 1) { // TAULA PUNTS I AILLAMENTS
dummy = CAN_0.TIMER.R;
buffer_lectura = 8;

CAN_0.IFRL.B.BUF08I = 1;
}

if (CAN_0.IFRL.B.BUF09I == 1) { // TAULA CONTINUITAT
dummy = CAN_0.TIMER.R;
buffer_lectura = 9;

CAN_0.IFRL.B.BUF09I = 1;
}

if (CAN_0.IFRL.B.BUF10I == 1) { // TAULA CIRCUITS
dummy = CAN_0.TIMER.R;
buffer_lectura = 10;

CAN_0.IFRL.B.BUF10I = 1;
}

if (CAN_0.IFRL.B.BUF11I == 1) { // TAULA DETECCIONS
dummy = CAN_0.TIMER.R;
buffer_lectura = 11;

CAN_0.IFRL.B.BUF11I = 1;
}
nova_taula = 0;
}
else {
//Send_Head(CAN_0.BUF[buffer_lectura].DATA.B[0], Mis_Error, codi_test, 0, 1); // ENVIAR ERROR
CAN_0.IFRL.R |= 0x00000F00;
}
}


/*----------------- Rutina de servei a la interrupcio del CAN0 BUFFER 0-3 -------------------
* Interrupcio del PC per realitzar una nova comanda. General o particular. Amb o sense LOG's
--------------------------------------------------------------------------------------------*/
static void CAN0_ISR_COMANDES (void) { // Interrupcions CAN Buffer 0. Podem detectar que arrivi una operacio, abans d'acabar l'anterior

if (nova_operacio == 0) {
if (CAN_0.IFRL.B.BUF00I == 1) { // Comanda General + LOG
nova_operacio = 1;
buffer_lectura = 0;
LOGS++;
codi_test = CAN_0.BUF[buffer_lectura].DATA.B[1];
//dummy = CAN_0.BUF[buffer_lectura].CS.B.LENGTH; // Read the size of CAN message

CAN_0.IFRL.B.BUF00I = 1;
}
if (CAN_0.IFRL.B.BUF01I == 1) { // Comanda General
nova_operacio = 1;
buffer_lectura = 1;
codi_test = CAN_0.BUF[buffer_lectura].DATA.B[1];
//dummy = CAN_0.BUF[buffer_lectura].CS.B.LENGTH; // Read the size of CAN message

CAN_0.IFRL.B.BUF01I = 1;
}
if (CAN_0.IFRL.B.BUF02I == 1) { // Comanda Propia + LOG
nova_operacio = 1;
buffer_lectura = 2;
LOGS++;
codi_test = CAN_0.BUF[buffer_lectura].DATA.B[1];
//dummy = CAN_0.BUF[buffer_lectura].CS.B.LENGTH; // Read the size of CAN message

CAN_0.IFRL.B.BUF02I = 1;
}
if (CAN_0.IFRL.B.BUF03I == 1) { // Comanda Propia
nova_operacio = 1;
buffer_lectura = 3;
codi_test = CAN_0.BUF[buffer_lectura].DATA.B[1];
//dummy = CAN_0.BUF[buffer_lectura].CS.B.LENGTH; // Read the size of CAN message

CAN_0.IFRL.B.BUF03I = 1;
}
}
else {
//Error = 1;
//Send_Head(CAN_0.BUF[buffer_lectura].DATA.B[0], Mis_Error, 0x01, codi_test, 2); // ENVIAR ERROR
CAN_0.IFRL.R |= 0x0000000F;
}
}

//++++++++++++++++++++++++++++ PRINCIPAL +++++++++++++++++++++++++++++++++++++++++++++++++++++

int main(void)
{
int i = 0;

/* INICIALITZACIONS */
InitCMU_0(); // 8 MHz OSC requires non-default CMU_0 init
InitModesAndClks(); // Initialize mode entries
DisableWatchdog(); // Disable watchdog
initPeriClkGen();
InitGPIO(); // Initialize GPIO Pins

INTC_InstallINTCInterruptHandler(CAN0_ISR_TAULES,70,14); // INIT FlexCAN Interrupt MB 8-11
INTC_InstallINTCInterruptHandler(CAN0_ISR_COMANDES,68,13); // INIT FlexCAN Interrupt MB 0-3

EnableIrq(); // General Enable for ISR
Clr_LedErr();
Set_LedAlim();


// LLEGIR DEL POTENCIOMETRE EL ID
ID = 49; // ID = Carta
ID_Buffers = ID<<4; // ID_Buffers = Carta + 0000

// CONFIGURAR CAN UN COP TENIM EL ID
InitCAN_0();
InitCAN_1();

/* TEST */
while (1)
{
if (nova_operacio) // Nova operacio. Cada interrupcio del BUF04 de CAN
{
nova_operacio = 0;
//dummy = CAN_0.BUF[buffer_lectura].CS.B.LENGTH; // Read the size of CAN message
}
}
}

1 Solution
1,272 Views
martin_kovar
NXP Employee
NXP Employee

Hello,

the problem is, that when you read the length of the message, you lock message buffer and this remains lock. Please check the the figure below:

pastedImage_1.png

I also recommend you to read chapter Mailbox lock mechanism.

If you have any other questions, please feel free to write me back.

Regards,

Martin

View solution in original post

1 Reply
1,273 Views
martin_kovar
NXP Employee
NXP Employee

Hello,

the problem is, that when you read the length of the message, you lock message buffer and this remains lock. Please check the the figure below:

pastedImage_1.png

I also recommend you to read chapter Mailbox lock mechanism.

If you have any other questions, please feel free to write me back.

Regards,

Martin