Hi. I am using MPC5644A and want to erase Flash memory by using C90FL Driver.
FlashErase have Parameters(in) : lowEnabledBlocks, midEnabledBlocks, highEnabledBlock.
I don't know What I should put a data in lowEnabledBlocks, midEnabledBlocks, highEnabledBlock.
lowEnableBlocks | M1 | M0 | L9 | L8 | L7 | L6 | L5 | L4 | L3 | L2 | L1 | L0 |
data | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 |
midEnabledBlocks |
|
|
|
|
|
|
|
|
|
| M0 | L0 |
data |
|
|
|
|
|
|
|
|
|
| 0 | 0 |
highEnabledBlock |
|
|
|
|
| H6 | H5 | H4 | H3 | H2 | H1 | H0 |
data |
|
|
|
|
| 0 | 0 | 0 | 0 | 0 | 0 | 0 |
is it right????
if i want to erase 0x4000 Block, 0x1_0000 block, 0x0004_0000 block, 0x00C_0000 block, 0x0020_0000 block
What should I deal with lowEnabledBlocks, midEnabledBlocks, highEnabledBlock Parameters
MPC5644A flash memory
FlashErase Function
解決済! 解決策の投稿を見る。
No, it is not. With using of SSD driver, user uses logical address mapping. midEnabledBlock has only 2 bits.
I tried to erase Flash memory '0x3_0000~ 40_0000' to use Function 'pFlashErase' (0x0000~0x3_0000 is Bootloader)
I set
lowEnabledBlocks = 0xE00 = 0b1110_0000_0000
midEnabledBlocks = 0x3 = 0b11
highEnabledBlock = 0x3F = 0b11_1111
but the area '0x4_0000~0x6_0000' and 0x3F_0000..' is not erased..(check it by trace32)
I tried again
lowEnabledBlocks = 0xFFFF_FFFF
midEnabledBlocks = 0xFFFF_FFFF
highEnabledBlock = 0xFFFF_FFFF
and the area '0x4_0000~0x6_0000' and 0x3F_0000..' is erased exactly.
What is the problem??
Thank you for your help
I have just it and it works normally to me.
lowEnabledBlocks = 0x0E00 followed by erase sequence erases 0x0003_0000-0x0007_FFFF
I don't see any issue.
Thank you very much
it works well
Yes, it is right if you mean physical to logical address mapping.
Only I would note that the logical block is being selected by logic 1 in the particular bit-mapped position.
midEnabledBlock is L0 and M0 of Flash B??
As you say, midEnabledBlock is just 2 bit ??
but in Datasheet MPC5644A
High-Address Space Block Select Register is 10bit
Mid-Address Space Block Select Register is 2bit
Low-Address Space Block Select Register is 6bit
is this not relevant????
No, it is not. With using of SSD driver, user uses logical address mapping. midEnabledBlock has only 2 bits.