I tried to flash the MPC5744P using CAN and I used a CAN case for that, and I configured both the pins and baud rate as required, but it didn't flash the file and I received the following message.
Are there any missing steps to flash the kit successfully using CAN ?
Is it the vector CAN case which is used to flash the kit ??
It flashed using CAN when I changed the following
flash_rchw : org = 0x00FA0000, len = 0x4
cpu0_reset_vec : org = 0x00FA0004, len = 0x4
delay_us : org = 0x00FA0008, len = 0x4
appkey_addr : org = 0x00FA000C, len = 0x4
But the applications doesn't work
when I Flashed using serial UART 0 the previous version of the rbf
the application worked when I write as
flash_rchw : org = 0x00FC0000, len = 0x4
cpu0_reset_vec : org = 0x00FC0004, len = 0x4
delay_us : org = 0x00FC0008, len = 0x4
appkey_addr : org = 0x00FC000C, len = 0x4
any help with that ?
Or maybe @mikedoidge , do you have an idea what could be wrong if it is not caused by hardware?
Thanks,
Lukas
@lukaszadrapa any ideas regarding this issue?
could you please attach an application (srec file) to try it just in case if the issue in the application ?
Thank you
Hello,
from the attached screenshot it is obvious that the communication has been established.
Seems the Erasing process is being interrupted and causes the communication error.
Could you possibly try to dump some flash memory content ("Read Memory Content" e.g from 0xFC0000 - 0xFC1000).
Is it the only device on CAN bus? If not can you double check if it does not interfer with other messages with can ID 0?
Hope it helps.
Stan
Never mind,
Yes there is External wdg SBC,
Development board Dev NXP5744P Rev E
any certain connection should I do?
Thank you
@lukaszadrapa Yes , Debug mode is enabled
Hi,
see please this HOWTO article:
And you can use this latest version of RBF:
Regards,
Lukas