Boolean Set to an Illegal Value

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Boolean Set to an Illegal Value

652 Views
peterb2
Contributor III

We think we have found a bug with code warrior V2.10 when compiling for the MPC5534.  The bug is that sometimes a member variable bool of a class will be set to a value of 0xFF instead of 0x01.  Attached is example code for how to reproduce the problem.  The problem occurs in the constuctor of Test2 when it is assigning a value into bad_val as a a result of anding itself with success.

Test2 Constructor Dissassembly

48 00        se_li   r0,0
7c 00 00 34  cntlzw  r0,r0
00 c4        se_extzb r4
68 50        se_srwi r0,5
46 40        se_and  r0,r4
7c 80 00 d0  neg     r4,r0
44 40        se_or   r0,r4  // Here is the problem r0 is now 0xFFFFFFFF
66 00        se_btsti r0,0
48 14        se_li   r4,1
90 43        se_stb  r4,0(r3)
91 03        se_stb  r0,1(r3) // And bad_val gets assigned with 0xFF
e6 06        se_beq  3bca0 <__ct__5Test2Fb+0x26>
71 04 e0 86  e_lis   r8,8326
54 88 1c c0  e_stw   r4,7360(r8)
e8 06        se_b    3bcaa <__ct__5Test2Fb+0x30>
71 04 e0 86  e_lis   r8,8326
48 20        se_li   r0,2
54 08 1c c0  e_stw   r0,7360(r8)
00 04        se_blr
‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍

I tried to reproduce the problem for you in an example project.  Unfortunately the previous person who set this up is using a perl script to pass in all the compiler options to the IDE.  My problem at the moment is can't seem to line all of them up to whats in the software.  But I have it close and when it compiles this code it produces something very similar.  Plus it has an extra instruction before storing the value in to bad_val that makes it equal 1 instead of 0xFF and it makes everything work.  Hopefully this missing instruction can act like a clue for you?

48 15        se_li   r5,1
90 53        se_stb  r5,0(r3)
48 00        se_li   r0,0
00 c4        se_extzb r4
7c 00 00 34  cntlzw  r0,r0
68 50        se_srwi r0,5
46 40        se_and  r0,r4
7c 80 00 d0  neg     r4,r0
44 40        se_or   r0,r4
69 f0        se_srwi r0,31  // Shifts R0 to be 1 and this is what gets written in to bad_val
91 03        se_stb  r0,1(r3)
22 00        se_cmpli r0,1
e2 06        se_bne  2226 <__ct__5Test2Fb+0x28>
71 08 e0 01  e_lis   r8,16385
54 a8 f0 00  e_stw   r5,-4096(r8)
e8 06        se_b    2230 <__ct__5Test2Fb+0x32>
48 20        se_li   r0,2
71 08 e0 01  e_lis   r8,16385
54 08 f0 00  e_stw   r0,-4096(r8)
00 04        se_blr

If there is a document that talks about how to call the IDE from the command line for setting these compiler options, could you please share it with me?  It would help line up some of the compiler options.

Attached Files:

* test.cpp - Contains the relevant constructor that is producing the bad code

* test.h - Header file for it.

* main.cpp - Should be able to copy this in to a fresh project

* test.mcp - My current project file with my guesses as to what some of the compiler config is.

* MPC5534.lcf - A modified linker file I was using

If there is any other info you need please let me know.

0 Kudos
1 Reply

512 Views
peterb2
Contributor III

Also could I know the conditions in which the error occurs to safely work around it?

0 Kudos