Bit is reserved,Value must remain 1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Bit is reserved,Value must remain 1

607 Views
frank747
Contributor II

Hi all:

"Bit is reserved,and must not be writeen or cleared,Value must remain 1."

If the bit with the above description is changed to 0 by the software, what effect might it have?

MPC5125RM.pdf 5.3.1.2 Figure 5-7

Tags (1)
0 Kudos
Reply
1 Reply

600 Views
Pavel
NXP Employee
NXP Employee

Usually incorrect setting reserved bits can produce unpredictable behavior. Often these bits are used for different testing on the factory.

0 Kudos
Reply