Binary generation error on MPC5674F(CW 10.7)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Binary generation error on MPC5674F(CW 10.7)

1,607件の閲覧回数
hyenongijeong
Contributor III

Hi,

 

I need to use internal Flash area internal_flash:0x10_0000.

But I met under message.

When I use internal_flash area under 0x10_0000. It's good and no problem to make binary.

Description Resource Path Location Type
Can't write binary file 'FLCC_TPS.bin' because gap between bin file offset for segments .bss and .__bam_bootarea wasn't updated correctly (too much). FLCC_TPS C/C++ Problem

0 件の賞賛
返信
2 返答(返信)

1,514件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hello,

I checked your question, but unfortunately, I do not understand it well. Could you please clarify your question and share your linker file and map file of your project?

Regards,

Martin

0 件の賞賛
返信

1,514件の閲覧回数
hyenongijeong
Contributor III

Hi,

This problem is resolved my myself.

The problem was caused by the incompatible ROM address of the CW and the .text section of ".lcf".

Regards,

Henk