Adddres shift with APS=1 and PS=1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Adddres shift with APS=1 and PS=1

4,058 Views
marcellobellini
Contributor I

I have another strange problem sull'EBI: I set in OR0, APS = 1 and  PS=1 in BR0.  I have a bus 16-bit not multiplexed

I expect ADDRESS 31 (D_CS2 PIN) make ADDRESS 30, but it does not work well

Labels (1)
0 Kudos
Reply
13 Replies

3,781 Views
marcellobellini
Contributor I

i have dowload new mpc5777c user manual, also in new version CS2 is indicated

Address [31]

why in my application not work as Address [31]??

0 Kudos
Reply

3,781 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

We contacted the design person and confirmed that APS feature is implemented on mpc5777c device.

 

Please check the MCR, BR and OR register settings. Can you please share with me these register settings, particularly EBI_MCR[D16:31] value and D_CS2 SIU_PCR settings?

0 Kudos
Reply

3,781 Views
marcellobellini
Contributor I

Is possible send to me a schematic to connect EBI 16 bit bus non multiplexed to flash memory with APS=1(shift address)?

0 Kudos
Reply

3,781 Views
marcellobellini
Contributor I

i'm sure that aps=1 is implemented, but for use this parameter on OR, it is need work also CS2 set as addres A31

If the cpu bug that not set CS2 as address A31(with APS=1 get A30) is not possible use APS parameter

In new user manual this part is not change

manual indicate cs2 as address, but note 3 only data.

the correct value is address and not data.

0 Kudos
Reply

3,781 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

I have been just confirmed from the designer that table 27-3 entry for D_CS2 in non-muxed 16-bit mode is wrong and it is not connected to ADDRESS[31] but rather is hooked to DATA[31].

So unfortunately, APS feature is not useful in this mode.

Ticket for potential errata/RM update has been created. We're sorry for the inconvenience it might bring to you.

0 Kudos
Reply

3,781 Views
marcellobellini
Contributor I

i have a suspicion and with a program test is very probable:

in your user manual:

Table 27-3. Function of EBI pins for supported configurations

Non-muxed 16-bit mode PIN D_CS2 is Address [31]

but with test is an Data, not work as ADDRESS!!!!! 

Is possible a this BIG BUG IN CPU????????

0 Kudos
Reply

3,781 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, I don't have experience with this configuration as it is new feature, I will try to find out letting you know then.

0 Kudos
Reply

3,781 Views
marcellobellini
Contributor I

I do not understand if the transition from Freescale to NXP is the cause of tecnological and support  degradation on MPC5777C family. it is 'absurd not to have an answer on three problems in many months

1)test burst is easy on MPC5777C EVB

2)test dual core memory coerency, if i use SRAM on EBI  is easy for NXP in EVB

3)test APS=1 and D_CS2 if has address is very easy

0 Kudos
Reply

3,781 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

I am apologizing for not hearing from us. I can understand the inconvenience this might bring to you. Just for explanation:

1) This has been escalated relatively long time ago, but assigned person has been changed recently as previously assigned person probably left the company. Now it is assigned to another person. I have already urged him for solution.

2) This has been stucked on my side as I just forgot on your other thread. Once again sorry for that. When you give me details I will work on that with priority.

3) This is in progress on application engineer's side, I have also reported this in relation to obvious discrepancy in our RM where it is stated that D_CS2 pin function is Address[31] and note 3 before Table 27-3 says it is basically Data[31]. In normal circumstances this pin is not used as 16-bit or 32-bit memories does not connect this address lines so even in case it would not work as expected probably nobody would notice. It must be somehow solved and will be.

In general you are dealing with urgent issues I would rather recommend to create a case for it:
https://community.nxp.com/docs/DOC-329745

Thanks for undertanding

0 Kudos
Reply

3,781 Views
marcellobellini
Contributor I

NXP intends to revise the 5777C mask, settling the problems of the CS2 pin,  burst problem and  the Platform coherency Unit in dual core mode when core 1 work in memory on EBI?

0 Kudos
Reply

3,781 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

You have told in thread 438364:
“I will prepare some documentation and C example.”
Have you created such one? Could you share it with us?


I have no idea what application engineers/designers will decide to do with that but we really need as much information as possible from your side.
If you already create a case how I recommended in previous answer, please give me its number. Thanks

0 Kudos
Reply

3,781 Views
marcellobellini
Contributor I

for the PCU problem I have try to generate a simple C code, becuse is not easy with two core and EBI.
However, in testing I found that the PCU registers do not even report the overflow in the specific bits for example

on

CP1ERR[1:0] CP0ERR[1:0]

for APS=1 i not have soluction or workaround

0 Kudos
Reply

3,781 Views
marcellobellini
Contributor I

ok, thank you

0 Kudos
Reply