About Processor Packages for MPC5748

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About Processor Packages for MPC5748

413 Views
2271157674
Contributor I

hello everybody,

I use S32DS to develop MPC5748G.

how do you chang the Processor Packages of the created project. I want it to be MPC5748G_176 in LQFP176 152-pin package, but it's only MPC5748G_324 in MAPBGA324 271-pin package.How should i change the Processor Packages?屏幕截图.png

Labels (1)
0 Kudos
1 Reply

314 Views
martin_kovar
NXP Employee
NXP Employee

Hello,

please see the tutorial below. It is determined for S32k microcontrollers, but there are the same steps for Power Architecture microcontrollers.

https://community.nxp.com/docs/DOC-334936 

Please let me know, if you have any issue with the tutorial.

Regards,

Martin

0 Kudos