hello, Do you have some datasheet about the instructions which are used in the 57xxflash.ld file ?
Bellow is the example.
/* Entry Point */
ENTRY(_start)
/* define heap and stack size */
__HEAP_SIZE = 0 ;
__STACK_SIZE = 4096 ;
SRAM_SIZE = 96K;
/* Define SRAM Base Address */
SRAM_BASE_ADDR = 0x40000000;
/* Define CPU1 Local Instruction SRAM Allocation */
LOCALIMEM_SIZE = 16K;
/* Define CPU1 Local Instruction SRAM Base Address */
LOCALIMEM_BASE_ADDR = 0x51000000;
/* Define CPU1 Local Data SRAM Allocation */
LOCALDMEM_SIZE = 32K;
/* Define CPU1 Local Data SRAM Base Address */
LOCALDMEM_BASE_ADDR = 0x51800000;
MEMORY
{
flash_rchw : org = 0x00F9C000, len = 0x4
cpu0_reset_vec : org = 0x00F9C000+0x10, len = 0x4
cpu1_reset_vec : org = 0x00F9C000+0x14, len = 0x4
m_text : org = 0x1000000, len = 1280K
m_data : org = 0x40000000, len = 96K
local_imem : org = 0x51000000, len = 16K
local_dmem : org = 0x51800000, len = 32K
}
SECTIONS
{
.rchw :
{
KEEP(*(.rchw))
} > flash_rchw
.cpu0_reset_vector :
{
KEEP(*(.cpu0_reset_vector))
} > cpu0_reset_vec
.cpu1_reset_vector :
{
KEEP(*(.cpu1_reset_vector))
} > cpu1_reset_vec
/* Note: if you move the 'startup' section shall modify the RCHW2_1 value for the corresponding core in the flashrchw.c file. */
.startup : ALIGN(0x400)
{
__start = . ;
*(.startup)
} > m_text
.core_exceptions_table : ALIGN(4096)
{
__IVPR_VALUE = . ;
KEEP(*(.core_exceptions_table))
} > m_text
.intc_vector_table : ALIGN(4096)
{
KEEP(*(.intc_vector_table))
} > m_text
.text :
{
*(.text.startup)
*(.text)
*(.text.*)
KEEP (*(.init))
KEEP (*(.fini))
. = ALIGN(16);
} > m_text
.ctors :
{
__CTOR_LIST__ = .;
/* gcc uses crtbegin.o to find the start of
the constructors, so we make sure it is
first. Because this is a wildcard, it
doesn't matter if the user does not
actually link against crtbegin.o; the
linker won't look for a file to match a
wildcard. The wildcard also means that it
doesn't matter which directory crtbegin.o
is in. */
KEEP (*crtbegin.o(.ctors))
KEEP (*crtbegin?.o(.ctors))
/* We don't want to include the .ctor section from
from the crtend.o file until after the sorted ctors.
The .ctor section from the crtend file contains the
end of ctors marker and it must be last */
KEEP (*(EXCLUDE_FILE(*crtend?.o *crtend.o) .ctors))
KEEP (*(SORT(.ctors.*)))
KEEP (*(.ctors))
__CTOR_END__ = .;
} > m_text
.dtors :
{
__DTOR_LIST__ = .;
KEEP (*crtbegin.o(.dtors))
KEEP (*crtbegin?.o(.dtors))
KEEP (*(EXCLUDE_FILE(*crtend?.o *crtend.o) .dtors))
KEEP (*(SORT(.dtors.*)))
KEEP (*(.dtors))
__DTOR_END__ = .;
} > m_text
.preinit_array :
{
PROVIDE_HIDDEN (__preinit_array_start = .);
KEEP (*(.preinit_array*))
PROVIDE_HIDDEN (__preinit_array_end = .);
} > m_text
.init_array :
{
PROVIDE_HIDDEN (__init_array_start = .);
KEEP (*(SORT(.init_array.*)))
KEEP (*(.init_array*))
PROVIDE_HIDDEN (__init_array_end = .);
} > m_text
.fini_array :
{
PROVIDE_HIDDEN (__fini_array_start = .);
KEEP (*(SORT(.fini_array.*)))
KEEP (*(.fini_array*))
PROVIDE_HIDDEN (__fini_array_end = .);
} > m_text
.rodata :
{
*(.rodata)
*(.rodata.*)
} > m_text
.eh_frame_hdr : { *(.eh_frame_hdr) } > m_text
.eh_frame : { KEEP (*(.eh_frame)) } > m_text
.data :
{
*(.data)
*(.data.*)
} > m_data AT>m_text
.sdata2 :
{
*(.sdata2)
*(.sdata2.*)
} > m_data AT>m_text
.sbss2 (NOLOAD) :
{
/* _SDA2_BASE_ = .; */
*(.sbss2)
*(.sbss2.*)
} > m_data
.sdata :
{
*(.sdata)
*(.sdata.*)
} > m_data AT>m_text
.bss (NOLOAD) :
{
__BSS_START = .;
*(.sbss)
*(.sbss.*)
*(.bss)
*(.bss.*)
*(COMMON)
__BSS_END = .;
} > m_data
.stack (NOLOAD) : ALIGN(16)
{
__HEAP = . ;
PROVIDE (_end = . );
PROVIDE (end = . );
. += __HEAP_SIZE ;
__HEAP_END = . ;
_stack_end = . ;
. += __STACK_SIZE ;
_stack_addr = . ;
__SP_INIT = . ;
. += 4;
} > local_dmem
/*-------- LABELS USED IN CODE -------------------------------*/
/* Labels for Copying Initialised Data from Flash to RAM */
__DATA_SRAM_ADDR = ADDR(.data);
__SDATA_SRAM_ADDR = ADDR(.sdata);
__DATA_SIZE = SIZEOF(.data);
__SDATA_SIZE = SIZEOF(.sdata);
__DATA_ROM_ADDR = LOADADDR(.data);
__SDATA_ROM_ADDR = LOADADDR(.sdata);
/* Labels Used for Initialising SRAM ECC */
__SRAM_SIZE = SRAM_SIZE;
__SRAM_BASE_ADDR = SRAM_BASE_ADDR;
__LOCAL_DMEM_SIZE = LOCALDMEM_SIZE;
__LOCAL_DMEM_BASE_ADDR = LOCALDMEM_BASE_ADDR;
__LOCAL_IMEM_SIZE = LOCALIMEM_SIZE;
__LOCAL_IMEM_BASE_ADDR = LOCALIMEM_BASE_ADDR;
__BSS_SIZE = __BSS_END - __BSS_START;
}
Hello,
S32 Design Studio uses GNU GCC toolchain by default, so, you can use datasheet below for analyzing linker files.
https://www.eecs.umich.edu/courses/eecs373/readings/Linker.pdf
Regards,
Martin
Thank you very much !