AUTOSAR MCAL configiration for MPC5746RK1MLU3(176Pin)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

AUTOSAR MCAL configiration for MPC5746RK1MLU3(176Pin)

Jump to solution
878 Views
fedotech
Contributor II

Hello!

I'm configuring MPC5746R using MPC574XR_MCAL4_0_RTM_1_0_3. The chip part number is SPC5746RK1MLU3 which is 176LQFP package. But, I can't find this derivative in the MCAL resource module. Should I select mpc5745r_lqfp176?

Autosar Resource ModuleAutosar Resource Module

Thanks!

 

0 Kudos
Reply
1 Solution
846 Views
cuongnguyenphu
NXP Employee
NXP Employee

Hi @fedotech , 
Current MPC574XR_MCAL4_0_RTM_1_0_3 package doesn't support for mpc5746R_lqfp176 as Release Note.
But I think you can use mpc5745r_lqfp176 as derivative because there's not much difference between these 2 targets. Only difference between Flash (5746R has 4256 KB, 5745R has 3232KB) and RAM size (5746R has 256 KB, 5745R has 192KB). So if your application use Flash or RAM, please be caution about Flash or RAM size because you couldn't config full size of Flash and RAM. Apart from this, everything is alright
Capture.PNG
For more information about difference of these 2 targets, you can check in Reference Manual document (Section 1.2.2 Feature list https://www.nxp.com/webapp/Download?colCode=MPC5746RRM&location=null

View solution in original post

1 Reply
847 Views
cuongnguyenphu
NXP Employee
NXP Employee

Hi @fedotech , 
Current MPC574XR_MCAL4_0_RTM_1_0_3 package doesn't support for mpc5746R_lqfp176 as Release Note.
But I think you can use mpc5745r_lqfp176 as derivative because there's not much difference between these 2 targets. Only difference between Flash (5746R has 4256 KB, 5745R has 3232KB) and RAM size (5746R has 256 KB, 5745R has 192KB). So if your application use Flash or RAM, please be caution about Flash or RAM size because you couldn't config full size of Flash and RAM. Apart from this, everything is alright
Capture.PNG
For more information about difference of these 2 targets, you can check in Reference Manual document (Section 1.2.2 Feature list https://www.nxp.com/webapp/Download?colCode=MPC5746RRM&location=null