AUTOSAR 4.3 MCAL (ISO 26262) for MPC5777C

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

AUTOSAR 4.3 MCAL (ISO 26262) for MPC5777C

1,505 Views
PENGHAN
Contributor II

Dear:

     I want to use the AUTOSAR configuration tool to config to the MCAL of MPC5777C.This is the Download Information that I search on nxp official website.1.PNG2.PNG

But I don't know what these two parts are and how to install and use,Are there installation instructions and software instructions available and referenced?Sincerely need your help, thank you very much.

respectly

0 Kudos
Reply
3 Replies

1,460 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

In 1.0.1 there is no example code. But if you take 1.0.0 there is example code.

So how can the driver source code in the MCAL file be used by EB software?

This is more theme for MCAL training, but you simply create new project, add plugins which you will use, set up pluggins and generate code.

Then you need to put files in some project manager (for example GHS) and compile the code.

Its hard to start from scratch with no training, but it is possible.

Best regards,

Peter

0 Kudos
Reply

1,480 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Instalation is pretty simple.

1. install EB tresos

2. Install MCAL for your device + generate license on the same page as installation package is.

This is all you need to setup the project.

About SW instruction. each plugin contains documentation for functions.

 

Example is not in MPC5777C RTM, 1.0.1.

But you can find one in RTM 1.0.0

 

best regards,

Peter

0 Kudos
Reply

1,478 Views
PENGHAN
Contributor II

Dear 

  I have installed EB tresos software and MPC5777C chip MCAL (MPC5777C_MCAL4_3_RTM_1_0_1). But there is no project in MCAL for EB software to load. So how can the driver source code in the MCAL file be used by EB software?

The following figure is the installation directory of MCAL.1.PNG

0 Kudos
Reply