ADC Input Voltage Range of MPC5744P-DEVKIT

cancel
Showing results for 
Search instead for 
Did you mean: 

ADC Input Voltage Range of MPC5744P-DEVKIT

Jump to solution
520 Views
ykarata1
Contributor IV
Dear All, I will use MPC5744 DEVKIT and try to read Analog Voltage. In the documents I am confused with ADC input range. In some parts, I have seen 3.3V in some 5.0 V as reference. I need to use 5V input range. If it is 3.3V how can I change input range to 5V. If it is already 5V, It is OK for me. Thanks.
0 Kudos
1 Solution
510 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

MPC5744P supports both 3.3V and 5V voltage reference:

lukaszadrapa_0-1615883775528.png

Notice that both VDD_HV_ADRE0 and VDD_HV_ADRE1 need to be supplied by the same voltage source.

If you take closer look at the schematic (https://www.nxp.com/webapp/Download?colCode=SCH-29333-E), you will see:

lukaszadrapa_1-1615883939425.png

And:

lukaszadrapa_2-1615883996147.png

So, it can be easily configured as needed.

Regards,

Lukas

 

View solution in original post

1 Reply
511 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

MPC5744P supports both 3.3V and 5V voltage reference:

lukaszadrapa_0-1615883775528.png

Notice that both VDD_HV_ADRE0 and VDD_HV_ADRE1 need to be supplied by the same voltage source.

If you take closer look at the schematic (https://www.nxp.com/webapp/Download?colCode=SCH-29333-E), you will see:

lukaszadrapa_1-1615883939425.png

And:

lukaszadrapa_2-1615883996147.png

So, it can be easily configured as needed.

Regards,

Lukas