ADC External Trigger Pins for Eval Board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ADC External Trigger Pins for Eval Board

766 Views
mpc5676r
Contributor II

The queries on MPC5676R ADC are explained in detail in the attachment. Please look into them and reply as soon as possible.

Thank you

Labels (1)
0 Kudos
1 Reply

685 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

ETRIGx are external trigger signals to the eQADC module. Still it represents internal signals which source can be selected by the SIU.ISEL[4-7] registers. See chapter 3.2.1.18 and Table 3-27 to Table 3-38 of the device Reference manual.

For example Table 3-27. eQADC_A Command FIFO 0 Trigger Sources

pastedImage_7.png

So many PIT, eTPU and eMIOS channels can be selected and also you can locate 2 external signals called “eTRIG0 pin” and “eTRIG1 pin”. These are available on pads AF23 and AD6(AA8)

pastedImage_5.png

pastedImage_6.png

BR, Petr

0 Kudos