5748G static power consumption problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

5748G static power consumption problem

394 Views
jacst
Contributor II

We are on the 5748G DEMO board, do not perform any operation after power-on, and directly enter the standby mode. The actual measurement found that the power consumption is about 1.5mA. It is quite different from the following data. May I ask what could be the cause of this? Can this chip indeed achieve the following data? ?

0 Kudos
1 Reply

383 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

which board do you have exactly and where do you measure the current? Are you sure it is a current supplying only the MCU?

Regards,

Lukas

0 Kudos