5605B in place of the 5607B?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

5605B in place of the 5607B?

789 Views
ericcastle
Contributor I

We are currently using an NXP part on my program (SPC5607BK0VLQ6), but we cannot find it in stock anywhere. It looks like the SPC5605BK0VLQ6 should be a drop-in replacement: same form-factor, same peripherals, same software, etc.

It looks like the only differences are listed in Table 2-1 of the MPC5607B manual: FLASH (768 kB instead of 1.5 MB) and RAM (64 kB instead of 92 kB). I don’t actually see the MPC5607B 144 LQFP listed on this table, but I'm assuming that it would have the same peripheral count as the 5605 and 5606 144 LQFP.

Can anyone confirm that I can use the 5605B in place of the 5607B? (I'm fine with the FLASH and RAM differences)

Thanks!

Tags (2)
2 Replies

693 Views
ericcastle
Contributor I

Thanks, David!

0 Kudos
Reply

693 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

If you are OK with smaller internal memories, then you can use it as replacement in the same package. There is no other difference.