Hello,
I am using the MPC5642A microcontroller (XPC563M_XPC564A_176QFPMINI Rev. A, XPC56XX EVB MOTHERBOARD Rev. C) and I aim to read the voltage value from the ADC 8th channel (AN8).
RM seems to include AN8 in the 176 pin package. However, I cannot find which AN8 pin is on the development board.
I reviewed the documents and schematics below. However, I could not access the information from which pin to read this value.
XPC56xxMBSCH.pdf
xPC56XXMB_Freescale_User_Manual_v_1_05.pdf
Thanks.
I would recommend contacting PeMicro support as they can provide you with comprehensive support for their products:
http://www.pemicro.com/support/index.cfm
A CD was distributed with the MPC56xx EVB developed by PeMicro, and this CD contains all the documentation for all EVB variants (eg the MPC5644A minimodule and the description of the motherboard with respect to the MPC5644A signals). I'm pretty sure this pack was available for download on their website, but I can't find it at the moment.