MPC5xxx知识库

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MPC5xxx Knowledge Base

标签
  • General 164
  • test 7

讨论

排序依据:
MCU:MPC5606B External Crystal Oscillator: 9.6M System Core Frequency: 64MHz DSPI Baute rate: 1.14Mbps CPOL:0 CPHA:0 Receive\Transmit Interrupt:enable; attention:CONT   QQ:511437685
查看全文
******************************************************************************** * Detailed Description: * * Example shows how to trigger ADC conversion on falling edge of PWM signal. * eMIOS ch1 is set to SAIC mode and a flag generated on selected edge detection * triggers BCTU channel which starts conversion of ADC1 ch9. On this channel * the board's trimmer is connected. * * EVB connection: * * J3.1 .. PA[1] - connect external PWM signal * J3.3 .. PA[2] - toggled in BCTU interrupt after ADC measurement * * ------------------------------------------------------------------------------ * Test HW: DEVKIT-MPC5748G * Maskset: 0N78S * Target : FLASH * Fsys: 160 MHz PLL * Debugger: Lauterbach * ******************************************************************************** Revision History: 1.0 Nov-5-2019 Petr Stancik Initial Version *******************************************************************************/
查看全文
IDE: CodeWarrior 10.6 mcu:MPC5606B Conversion Mode:Scan Channel: ADC1, 1\2\3\13\14 End of Chain Conversion interrupt enable; QQ:511437685
查看全文