MPC5xxx Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5xxx Knowledge Base

Labels
  • General 164
  • test 7

Discussions

Sort by:
This demo performs a communication on LIN bus between two MPC5604B EVBs.   LinFlex0 LIN Master ******************************************************************************** * Detailed Description: * - send header from a LIN Master * - either receive data from a LIN Slave or transmit a data * - no interrupt is used, just SW pooling * * ------------------------------------------------------------------------------ * Test HW:  XPC560B 144 LQFP MINIMODULE, XPC56XX EVB MOTHERBOARD, SPC5604B 2M27V * Target :  internal_RAM, Flash * LinFlex0: Lin Master, 19200 baudrate * Fsys:     64 MHz PLL with 8 MHz crystal reference * * ------------------------------------------------------------------------------ * EVB connections and jumper configuration * * XPC56XX EVB MOTHERBOARD * for LinFlex0 connection to the MC33661 LIN transceiver: * - RXDA_SEL (near SCI !!!!) jumper over pins 1-2 * - TXDA_SEL (near SCI) jumper over 1-2 * * for LIN Master functionality * - VSUP (J6) jumper fitted *   lin xceiver will get +12V from the EVB * - V_BUS (J14) jumper not fitted * - MASTER_EN jumper fitted * - LIN_EN jumper fitted * ********************************************************************************     LinFlex0 LIN Slave ******************************************************************************** * Detailed Description: * - receive header from a LIN Master * - either receive data from a LIN Master or transmit a data * - Filter can be enabled with the FILT_EN = 1 * - If filter is enabled TX interrupt is used to prepare data to send and *    RX interrupt to read received data * - If filter is disabled SW polling is used * * ------------------------------------------------------------------------------ * Test HW:  XPC560B 144 LQFP MINIMODULE, XPC56XX EVB MOTHERBOARD, SPC5604B 2M27V * Target :  internal_RAM * LinFlex0: Lin Slave, 19200 baudrate * Fsys:     64 MHz PLL with 8 MHz crystal reference * * ------------------------------------------------------------------------------ * EVB connections and jumper configuration * * XPC56XX EVB MOTHERBOARD * for LinFlex0 connection to the MC33661 LIN transceiver: * - RXDA_SEL (near SCI !!!!) jumper over pins 1-2 * - TXDA_SEL (near SCI) jumper over pins 1-2 * * for LIN Slave functionality * - VSUP (J6) jumper not fitted ...LIN transceiver will get +12V from the Master * - V_BUS jumper not fitted * - MASTER_EN jumper not fitted * - LIN_EN jumper fitted * ********************************************************************************
View full article
******************************************************************************** * Detailed Description: * In case user want GHS to initialize all cores it is necessary to define * preprocessor symbol: init_cores * However in this example the cores are initialized from function: Core_Boot(); * This example demonstrates how to initialize clock module and activate core0, core1 and core0 locksteped core. * ------------------------------------------------------------------------------ * Test HW:  MPC57xx EVB * Maskset:  0N78H * Target :  internal_FLASH * Fsys:     200 MHz PLL * ******************************************************************************** Revision History: 1.0     Feb-08-2016     b21190(Vlna Peter)  Initial Version 1.1    Feb-09-2016     b21190(Vlna Peter)  Added Core_Boot() function *******************************************************************************/
View full article
This example follows application notes AN3283 and AN4365. It is intended for users who develop own JTAG programmer. It shows how to implement basic functions: - enter debug mode during reset - enable external debug mode - OnCE access to GPR, SPR and memory - Nexus access to memory The example is written in PRACTICE script language using Trace32 debugger from Lauterbach (www.lauterbach.com). Low level functions for JTAG are used, so users can see sequences of ‘0’s and ‘1’s which are sent to JTAG interface. Used commands are described in this document: www2.lauterbach.com/pdf/general_ref_j.pdf This example was tested on MPC5607B device and VLE instruction set was used for OnCE access.
View full article
******************************************************************************** * Detailed Description: * * ECSM Error Generation Register EEGR is used to generate a non-correctable * or single bit ECC error in RAM. The bad data is accessed then, so the IVOR1 * exception is generated and handled. * This file shows also ECSM_combined_isr and how to correct the wrong data. * Use macro Induce_ECC_error_by_DMA_read to select whether ECC error will be * injected by DMA read or CPU read. * At the end of main file you can choose if single bit or multi bit is injected * and select particular ME/EE setup by comment/uncomment of particular function * calls. * * ------------------------------------------------------------------------------ * Test HW:   XPC567XKIT516 - MPC5674ADAT516 Rev.C, MPC567XEVBFXMB Rev.B * MCU:       PPC5674FMVYA264 * Terminal:  19200-8-no parity-1 stop bit-no flow control on eSCI_A * Fsys:      264/200/150/60 MHz * ********************************************************************************
View full article
******************************************************************************** * Detailed Description: * Purpose of the example is to show how to generate Multi bit ECC error in * internal SRAM or FLASH (user must choose it in the option at the end of main * function) and how to handle this error with respect to constraints given by * MPC5643L architecture (ECSM/RGM/FCCU relation and ECC error handling through * reset). The example is only possible to run in internal_FLASH target. Power- * -on-reset is required after downloading the code into MCU's flash. The example * displays notices in the terminal window (setting specified below). No other * external connection is required. * ------------------------------------------------------------------------------ * Test HW:         xPC564xLKIT, PPC5643L Cut3 silicon * Target :         internal_FLASH * Fsys:            120 MHz PLL0 * Debugger:        Lauterbach Trace32 *                  PeMicro USB-ML-PPCNEXUS * Terminal:        19200-8-no parity-1 stop bit-no flow control via LINFlex0 * EVB connection:  default * ********************************************************************************
View full article
******************************************************************************** * Detailed Description: * Application performs basic initialization, setup PLL to maximum allowed freq., * initializes interrupts, blinking one LED by interrupt, second LED by software * loop, initializes and display notice via UART terminal and then terminal ECHO. * The example configures the device for maximum performance (OPTIMIZATIONS_ON). * For XPC567XKIT516 it initializes EBI for mounted external SRAM device. * * ------------------------------------------------------------------------------ * Test HW:         XPC567XKIT516 - MPC5674ADAT516 Rev.C, MPC567XEVBFXMB Rev.B * MCU:             PPC5674FMVYA264 * Terminal:        19200-8-no parity-1 stop bit-no flow control on eSCI_A * Fsys:            264/200/150/60 MHz * Debugger:        Lauterbach Trace32 *                  PeMicro USB-ML-PPCNEXUS * Target:          RAM, internal_FLASH * EVB connection:  ETPUC0(J24-0) -> USER_LED_8 (J5-8) *                  ETPUC1(J24-1) -> USER_LED_7 (J5-7)(to see blinking LEDs) * ********************************************************************************
View full article
******************************************************************************** * Detailed Description: * Example show simple flash programming routine. During runtime it changes * content of field of constants 'test' (thus located in internal flash). * Also it shows how to relocate code into RAM a data into FLASH (used linker * command file is MPC5643L_my_sections.lcf and MPC5643L_DEBUG_my_sections.lcf). * * Note: For complex tasks use SSD driver (Freescale site for particular device, * Software&Tools/Run-Time Software/Middleware-Device Drivers * * ------------------------------------------------------------------------------ * Test HW:         xPC564xLKIT, PPC5643L Cut3 silicon * Target :         internal_FLASH, RAM * Fsys:            120 MHz PLL0 * Debugger:        Lauterbach Trace32 *                  PeMicro USB-ML-PPCNEXUS * Terminal:        19200-8-no parity-1 stop bit-no flow control via LINFlex0 * EVB connection:  default * ********************************************************************************
View full article
******************************************************************************** * Detailed Description: * Application performs basic initialization, setup PLL to maximum allowed freq., * initializes interrupts, blinking one LED by interrupt, second LED by software * loop, initializes and display notice via UART terminal and then terminal ECHO. * The example configures the device for maximum performance (OPTIMIZATIONS_ON) * by initialization of instruction/data cache and enabling of branch prediction. * Example suppose MCU is configured for DPM (Decoupled-parallel mode). * Its intention is to offer advanced startup code additional to CW stationery. * * ------------------------------------------------------------------------------ * Test HW:        MPC5675KEVB * MCU:            PPC5675KFMMSJ in Decoupled-parallel mode * Fsys:           180/150 MHz CORE_CLK * Debugger:       Lauterbach Trace32 *                 PeMicro USB-ML-PPCNEXUS * Target:         RAM, internal_FLASH * Terminal:       19200-8-no parity-1 stop bit-no flow control on eSCI_A * EVB connection: default * ********************************************************************************
View full article
******************************************************************************** * Detailed Description: * 200 MHz PLL with 40 MHz crystal reference + FCCU fault clearing *           example code + FCCU ALARM state configuration * ------------------------------------------------------------------------------ * Test HW:  MPC57xx Motherboard + MPC5744PE257DC minimodule, MPC5744P, * silicon mask set 1N65H * Target :  internal_FLASH* ********************************************************************************
View full article
******************************************************************************** * Detailed Description: * * CAN0 module is configured to transmit one message with ID 0x555 to CAN1 * module. CAN1 module is configured to use DMA to receive the message. * Once the DMA module reads the received frame, interrupt is triggered. * Follow application note AN4830 regarding the CAN settings. * http://www.freescale.com/files/microcontrollers/doc/app_note/AN4830.pdf * http://www.freescale.com/files/microcontrollers/doc/app_note/AN4830SW.zip * The example from AN4830 is modified to use DMA and RXFIFO on CAN1 module. * * ------------------------------------------------------------------------------ * Test HW:  MPC57xx * Maskset:  1N81M * Target :  SRAM * Fsys:     160 MHz PLL * ********************************************************************************
View full article
******************************************************************************** * Detailed Description: * Application performs basic initialization, setup PLL to maximum allowed freq., * initializes interrupts, blinking one LED by interrupt, * initializes and display notice via UART terminal and then terminal ECHO. * ------------------------------------------------------------------------------ * Test HW:        XPC5604B 100LQFP, XPC56XX EVB MOTHEBOARD Rev.C * MCU:             PPC5604BE MLL 1M27V * Fsys:             64/48 MHz * Debugger:      Lauterbach Trace32 *                      PeMicro USB-ML-PPCNEXUS * Target:          internal_FLASH, (not enough memory for RAM target) * Terminal:       19200-8-no parity-1 stop bit-no flow control on LINFLEX_0 * EVB connection: default * ********************************************************************************
View full article
******************************************************************************** * Detailed Description: * This example shows, how to communicate with RTC module PCA8565TS/1 via I2C bus. * For this purpose is used I2C driver created by Petr Stancik. Information from * RTC are sent using DMA via UART. The whole example consists from two parts. * Second part is PC application called GraphicalTerminalExample. This application * handles data from RTC and displays them. RTC also can be set using PC application. * Microcontroller receives data from PC application using DMA via UART. * Received data are written to RTC module. * * UART connection parameters: * Baud rate 19200b/s * 8 data bits * 1 stop bit * none parity * * For correct function of java application, it is required Java 1.8.0_40 * * ------------------------------------------------------------------------------ * Test HW:         MPC5775K-356DS, MPC57xx Motherboard * MCU:             PPC5775KMMY3B 0N76P * Fsys:            PLL0 266MHz *                    Z4 Core 133MHz * Debugger:        Lauterbach Trace32 *                  PeMicro USB-ML-PPCNEXUS * Target:          internal_FLASH (debug mode, release mode) * EVB connection: *                     UART connection *                     J14.1 connected to P12.6 (RX) *                     J13.1 connected to P12.7 (TX) * *                     RTC connection *                     RTC pin 4 - connected to any GROUND pin *                     RTC pin 8 - connected to any 3.3V pin *                     RTC pin 6 - connected to P8.10 (SCL - I2C clock) *                     RTC pin 5 - connected to P8.11 (SDA - I2C data) * ********************************************************************************
View full article
******************************************************************************** * Detailed Description: * * Simple LINFlex UART mode transmit and receive without interrupts (polled UART) * TXFIFO and RXFIFO macro is used to select between buffer and FIFO mode * * PIT channel 0 is also used to generate 1sec interrupt where PA0 pin is toggled. * * EVB connection: * *   Motherboard *   J14 - SCI_RX OFF *   J13 - SCI_TX OFF *   J25 - SCI_PWR ON * * See results on PC terminal (19200, 8N1, None). * ------------------------------------------------------------------------------ * Test HW:  MPC5777M, MPC57xx Motherboard + MPC5777M_512DS minimodule * Maskset:  0N78H * Target :  RAM, internal_FLASH * Fsys:     600 MHz PLL1 with 40 MHz crystal reference, *        core2 at 200MHz generated from PPL1 * Terminal: 19200, 8N1 ********************************************************************************
View full article
******************************************************************************** * Detailed Description: * Example configures LinFlex and eDMA modules and then periodically sends notice * to the terminal window (19200-8-no parity-1 stop bit-no flow control). * * ------------------------------------------------------------------------------ * Test HW:         MPC5607BEVB * Target :         internal_FLASH, RAM * Terminal:        19200-8-no parity-1 stop bit-no flow control * Fsys:            40 MHz PLL with 8 MHz crystal reference * Debugger:        Lauterbach Trace32 *                  PeMicro USB-ML-PPCNEXUS * Terminal:        19200-8-no parity-1 stop bit-no flow control via LINFlex0 * EVB connection:  default * ********************************************************************************
View full article
******************************************************************************** * Detailed Description: * This example shows, how to use interrupt hardware vector mode. In the example * PIT0 interrupt and external interrupt source 1 are implemented. PIT interrupt * toggle LED every second, external interrupt causes IVOR1 exception. * * This example also shows, how to use exceptions, while HW vector mode is used. * After SW1 button is pressed, uninitialized RAM is read and IVOR1 exception is * reached. In IVOR1, only endless loop is implemented and micro has to be reset * externally if you want to get out from this loop. * * * For correct HW vector mode setup, following files was added to the project: * *  - exceptions.s *  - handlers_vle.s *  - HW_vector.c * * * Following files was modified (all changes are marked by comment): * *  - mem.ld *  - sections.ld *  - Vector.c *  - MPC57xx__Interrupt_Init.c * * *  Following files was removed from project (files are still place in project, but *  not compiled and linked) * *  - intc_sw_handlers.S *  - intc_SW_mode_isr_vectors_MPC5744P.c * * * * Test HW:         X-MPC5744P-144DC, MPC57xx motherboard * MCU:             PPC5744PFMLQ8 0N15P * Fsys:            200 MHz * Debugger:        Lauterbach Trace32 *                  PeMicro USB-ML-PPCNEXUS * Target:          internal_FLASH (debug mode, release mode) * EVB connection:  User LED 1 connected to A0 (P8.0), *                    User switch SW1 connected to A1 (P8.1) * * * ------------------------------------------------------------------------------ * ********************************************************************************
View full article
******************************************************************************** * Detailed Description: * Enable external interrupt on pin PA[3]. * If falling edge is detected, interrupt is triggered and LED1 on PE[4] is * toggled. * * Connect external signal to PA[3] or connect push button by wire. * * ------------------------------------------------------------------------------ * Test HW:  TRK-MPC5606B, SPC5606B 0N32E * Target :  internal_FLASH, RAM * Fsys:     64 MHz PLL with 8 MHz crystal reference * ********************************************************************************
View full article
******************************************************************************** * Detailed Description: * Example of core watchdog implementation on Cobra 55. It executes on core 0 * All the functions are in the file "watchdog.c" *WatchDogCreate(delay, FirstTimeout, SecondTimeout) -> create/configure the wathdog timer *WatchDogStart() -> start the watchdog timer *WatchDogService() -> acknowledge the watchdog timer * ------------------------------------------------------------------------------ * Test HW:         MPC5777C-416DS Rev.A + MPC57xx MOTHER BOARD Rev.C * MCU:             PPC5777CMM03 2N45H CTZZS1521A * Fsys:            PLL1 = core_clk = 264MHz, PLL0 = 192MHz * Debugger:        Lauterbach Trace32 * Target:          internal_FLASH * ********************************************************************************
View full article
******************************************************************************** * Detailed Description: * Purpose of the example is to show how to generate Multi bit ECC error in * internal SRAM or FLASH (user can choose it in the option at the end of main * function) and how to handle this error with respect to constraints given by * MPC5675K architecture (ECSM/RGM/FCCU relation and ECC error handling through * reset). The example is only possible to run in internal_FLASH target. Power- * -on-reset is required after downloading the code into MCU's flash. The example * displays notices in the terminal window (setting specified below). No other * external connection is required. * Example also shows impact of enabled cache (macro OPTIMIZATIONS_ON). * * ------------------------------------------------------------------------------ * Test HW:        MPC5675KEVB * MCU:            PPC5675KFMMSJ in Lock-Step mode * Fsys:           180/150 MHz CORE_CLK * Debugger:       Lauterbach Trace32 *                 PeMicro USB-ML-PPCNEXUS * Target:         RAM, internal_FLASH * Terminal:       19200-8-no parity-1 stop bit-no flow control on eSCI_A * EVB connection: default * ********************************************************************************
View full article
******************************************************************************** * Detailed Description: * * * This example demonstrate functionality of XBIC_1 error injection *  capability. The fault is generated on DMA transfer to SRAM. *  After fault generation it is propagated to FCCU unit as NCF[59]. * * ------------------------------------------------------------------------------ * Test HW:  MPC57xx * Maskset:  1N65H * Target :  internal_FLASH * Fsys:     200 MHz PLL with 40 MHz crystal reference * ********************************************************************************
View full article
This document shows, how to use CRC gen utility in CodeWarrior for MCU IDE.   1) Create new project in CodeWarrior. 2) Create a file calc_crc.crc in the Project/Project_Settings/Linker_File directory. 3) Open project settings, choose C/C++ Build ->Settings and add the following command to Post-build steps: "${MCU_TOOLS_HOME}/bin/crcgen.exe" "${BuildLocation}/${BuildArtifactFileName}" -crc "${ProjDirPath}/Project_Settings/Linker_Files/calc_crc.crc" -srec "${BuildLocation}/${BuildArtifactFileName}.crc.mot" 26   4) Open calc_crc.crc and configure required parameters. Meaning of single lines is described in CodeWarrior reference manual called Targeting_Microcontrollers I used following code (it is only example)   5) Build your project. 6) File MPC5604B-CRCTest.elf.crc.mot was created   Now you have s-record, which contains CRC and which could be loaded to microcontroller.
View full article