******************************************************************************** * Detailed Description: * Initializes eQADC module, performs calibration and cyclically converts PMC * internal channel as specified by macros CHOOSEN_PMC_ADC_CHNL, * CHOOSEN_PMC_ADC_SCALE and CHOOSEN_PMC_ADC_COMMAND to check particular voltage * level, displaying it into terminal window. * Example configures decimation filter to scale signal down by 1/16, this is * achieved by FIR filter (user could choose real filter by proper coeficient * selection). * Example also sums filtered samples by integrator that is configured to be * triggered and zeroed by eTPU signal (for simplicity it uses general purpose * outputs). Integrated values are displayed in terminal window as well. * No external connection required excluding terminal via eSCI. * ------------------------------------------------------------------------------ * Test HW: XPC567XKIT516 - MPC567xADAT516 Rev.D, MPC567XEVBFXMB Rev.C * MCU: PPC5676RDMVY1 3N23A * Terminal: 19200-8-no parity-1 stop bit-no flow control on eSCI_A * Fsys: 180MHz * Debugger: Lauterbach Trace32 * PeMicro USB-ML-PPCNEXUS * Target: RAM, internal_FLASH * EVB connection: default ********************************************************************************
記事全体を表示