********************************************************************************  * Detailed Description:  * Application performs basic initialization, setup PLL to maximum allowed freq.,  * start one Z7 core, interrupts initialization, ICache and DCache are disabled  * on both cores because of shared memory, which must not be cached.  *  * There is 4K shared memory defined in the linker file. This memory is used by  * both cores. Both cores access into the structure, which is placed in the shared  * memory. This access is marked as a critical section. Only one core can write  * to the structure at the same time. To ensure this, there are Gates, which  * guarantee data coherence during the access. Only one core can be in critical  * section. Second core has to wait, until first core leaves the critical section  *  *  *  * ------------------------------------------------------------------------------  * Test HW:         MPC5775K-356DS, MPC57xx Motherboard  * MCU:             PPC5775KMMY3B 0N76P  * Terminal:        19200-8-no parity-1 stop bit-no flow control on LINFlexD_0  * Fsys:            PLL0 266MHz  *                    Z4 Core 133MHz  *                    Z7 Core 266MHz  * Debugger:        Lauterbach Trace32  *                  PeMicro USB-ML-PPCNEXUS  * Target:          internal_FLASH (debug mode, release mode)  * EVB connection:  default connection  *  ********************************************************************************   
        
        View full article