Using the Built-in Self-Test (BIST) on the MPC5744P

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using the Built-in Self-Test (BIST) on the MPC5744P

Using the Built-in Self-Test (BIST) on the MPC5744P

A requirement of the standard is to detect the accumulation of latent defects. To meet this requirement the MPC5744P has the ability to execute Built-In Self-Test (BIST) procedures.

Attachments
Comments

Hello Peter,

We have read the above BIST Application Note and the MPC5744P Safety and Reference Manuals, and our understanding is that the off-line BIST (MBIST and LBIST) is per default enabled and if any fault is detected the HW ensures that MCU stops executing (stays in reset). 

Can you please confirm that our understanding is correct?

Also, is there any way to verify this (e.g. inspecting UTEST flash area or injecting any fault to be detected by the off-line BIST)?

Best Regards,

Peder Rogö

Hi,

Yes, your understanding is correct.

For injecting the fault to BIST you can play with voltage during tests for example.

PS: if you have any questions create separate thread.

This one is intended only for issue found in my document.

Peter

No ratings
Version history
Last update:
‎06-06-2017 04:41 AM
Updated by: