MPC5777C - Online BISTs

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5777C - Online BISTs

MPC5777C - Online BISTs

This document describes how to use On-line BISTs on MPC5777C.

---------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------

STCU2 On-line BIST (MBIST+ LBIST) execution time on NXP Evaluation board ( X-MPC5777C-561DS) is 25.8ms.

This measured time is valid for:

System clock PLL = 200MHz

STCU module clock = System clock / 4

MBIST = 50MHz

LBIST = 25MHz

pastedImage_1.png

Result after testing MBIST+LBIST = 0 faults latched in ERR_STAT register and all LBISTs was successfully executed.

pastedImage_2.png

---------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------

STCU2 On-line LBIST only execution time on NXP Evaluation board ( X-MPC5777C-561DS) is 37.4ms.

pastedImage_3.png

pastedImage_4.png

This measured time is valid for:

System clock PLL = 200MHz

STCU module clock = System clock / 4

LBIST = 25MHz

---------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------

LBIST on 50MHz

I do not recommend to run LBIST at 50MHz as it was failing in my setup.

pastedImage_5.png

pastedImage_6.png

添付
コメント

I've tried to test code that you have attached, including that in my code. I'm not able to verify registers (as you have showed in this document) because as soon as the code enter in function STCU2_Online_BIST there is a reset. I'm using a JTAG connection with Lauterbach. Have you any suggestion?

Hi,

Please do not spam my example codes with comments.

Create new thread with reference to my example codes, but if you do not found any issue in my code do not post it here.

I have verified these example codes on 3 samples and all were running fine.

Besides I see you do not fully understand tests mechanism.

If test is started it takes cca 10-20ms to finish of execution. Then reset is generated after last LBIST. After reset you can attach debugger and read registers.

Peter

PS: I will delete those posts in a day.

Hello Peter,

I hope you're doing well, thank you for sharing this important thread. 

So, can you please share with us a script CMM of debug? 

Because at the start of the Built-in Self tests, a destructive reset is occured. 

after the reset is completed the report of the Built-in Self tests will be generated through LBESW and MBEHSW, MBEMSW, MBELSW. 

So I want to cover this transition and this reset in my script CMM without disconnecting the debugger means in trace32  (target in reset) 

100%が役に立ったと言っています (1/1)
バージョン履歴
最終更新日:
‎09-27-2017 04:03 AM
更新者: